how to modify flash_header for DDR3 2GB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to modify flash_header for DDR3 2GB

Jump to solution
1,812 Views
fangmingan
Contributor I

Based on mx6q_sabresd(default 1GB DDR3: 4x 2Gbit ddr3 chip, 64bit bus, only cs0 used  ), we want to change to 2GB DDR3, how to modify the flash_header.s

Thanks a lot

Original Attachment has been moved to: flash_header.S.txt.zip

Labels (1)
0 Kudos
Reply
1 Solution
1,157 Views
TaniaMartinez
Contributor III

Hello, We have a i.Mx6Q DDR3 programming register tool. This is a tool can generate a DDR3 script easily for i.Mx6DQSDL and only need input several parameters based on using DDR datasheet and system architecture.

Please find i.Mx6Q DDR3 Script Aid through below link.

https://community.freescale.com/docs/DOC-94917

Regards,

Tania

View solution in original post

0 Kudos
Reply
1 Reply
1,158 Views
TaniaMartinez
Contributor III

Hello, We have a i.Mx6Q DDR3 programming register tool. This is a tool can generate a DDR3 script easily for i.Mx6DQSDL and only need input several parameters based on using DDR datasheet and system architecture.

Please find i.Mx6Q DDR3 Script Aid through below link.

https://community.freescale.com/docs/DOC-94917

Regards,

Tania

0 Kudos
Reply