These packages failed to build: minicom

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

These packages failed to build: minicom

跳至解决方案
1,486 次查看
vishvapathi
Contributor V

Processing: minicom

=====================

Build path taken because: no prebuilt rpm,

Testing network connectivity

OK GPP:

Try minicom_2.2.orig.tar.gz from the GPP

Read error (Connection timed out) in headers.

Can't get: minicom_2.2.orig.tar.gz at ./ltib line 802.

f_buildrpms() returned an error, exiting

traceback:

main:572

Started: Wed Jul 17 11:59:59 2013

Ended:   Wed Jul 17 12:00:15 2013

Elapsed: 16 seconds

These packages failed to build:

minicom

Build Failed

Exiting on error or interrupt

Since there versions are updated the older once are not available i guess. How do i up date the ltib to look for the updated version in below link?

http://ftp.debian.org/debian/pool/main/m/minicom/minicom_2.6.2.orig.tar.gz


I have also manually downloaded the same to pkgs folder of LTIB, how do i make the LTIB to check the pkg folder instead of older version online.


Kindly advice

标签 (2)
0 项奖励
回复
1 解答
1,253 次查看
4guin4g4
Contributor IV

Modify the Makefile and Kconfig, to have ltib compile the new package.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,254 次查看
4guin4g4
Contributor IV

Modify the Makefile and Kconfig, to have ltib compile the new package.

0 项奖励
回复