how to implement the boot splash in u-boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to implement the boot splash in u-boot

2,742件の閲覧回数
DannyXiao
Contributor II

Dear all:

       I followed the chapter 10 in the document "13.5.0_Android_Advanced_User_Guide.pdf" and try to bring up the boot splash logo at uboot stage on MX6SL EVK board.

       But after I did all the things follow the steps in the document, I haven't seen anything on the EPD panel. Has anyone tried this?

ラベル(1)
6 返答(返信)

2,374件の閲覧回数
DannyXiao
Contributor II

Can anyone help on my question?

0 件の賞賛
返信

2,374件の閲覧回数
OtavioSalvador
Senior Contributor II

The 2013.07 U-Boot - going to be released very soon - has support for it.

2,374件の閲覧回数
DannyXiao
Contributor II

Thank you for your reply Otavio.  Is this 2013.07 u-boot the offical FSL release?

0 件の賞賛
返信

2,374件の閲覧回数
OtavioSalvador
Senior Contributor II

It is not. But it works wonderfully.

2,374件の閲覧回数
DannyXiao
Contributor II

Could you show me where to get this u-boot?

0 件の賞賛
返信

2,374件の閲覧回数
OtavioSalvador
Senior Contributor II

You can get it using GIT from:

git.denx.de Git - u-boot.git/summary

We also have it supported in the Yocto based BSP.

Yocto has a good community around it and currently most commonly used SoCs from i.MX platform is already supported by the meta-fsl-arm layer.


You can find more information how to make a build at https://community.freescale.com/docs/DOC-94023

i.MX Yocto Project: Frequently Asked Questions

0 件の賞賛
返信