how to enable the BT.1120 in imx6 linux BSP

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

how to enable the BT.1120 in imx6 linux BSP

2,426 次查看
huangjacky
Contributor III

Dear All:

I got the imx6 HW platform with ADV7441, the ADV7441 is HDMI ---> CSI encoder, support bt1120 interface.

Now I have confirm the i2c connect with ADV7441 is work.

I found the imx6 linux BSP is only support 8 or 10 bits bt.656, but found nothing with bt.1120.

refence the link: https://community.freescale.com/thread/303792

Qiang LiEmployee

For iMX6 BSP, the BT1120 16bits mode was not ready yet, we don't have the real hardware to enable it. Maybe you need reference to the iMX53 patch to support it.

I wanna know how to enable the bt.1120 function in imx6 linux BSP?

Thanks Advance!

标签 (3)
标记 (4)
2 回复数

1,420 次查看
YixingKong
Senior Contributor IV

Hi Jacky, please click Correct Answer/Helpful Answer, if your question had been answered.

Thanks,

Yixing

0 项奖励
回复

1,420 次查看
max_tsai
NXP Employee
NXP Employee

hi Jacky,

Please refer to https://community.freescale.com/docs/DOC-94019

-Max