how to enable the BT.1120 in imx6 linux BSP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to enable the BT.1120 in imx6 linux BSP

2,427 Views
huangjacky
Contributor III

Dear All:

I got the imx6 HW platform with ADV7441, the ADV7441 is HDMI ---> CSI encoder, support bt1120 interface.

Now I have confirm the i2c connect with ADV7441 is work.

I found the imx6 linux BSP is only support 8 or 10 bits bt.656, but found nothing with bt.1120.

refence the link: https://community.freescale.com/thread/303792

Qiang LiEmployee

For iMX6 BSP, the BT1120 16bits mode was not ready yet, we don't have the real hardware to enable it. Maybe you need reference to the iMX53 patch to support it.

I wanna know how to enable the bt.1120 function in imx6 linux BSP?

Thanks Advance!

Labels (3)
Tags (4)
2 Replies

1,421 Views
YixingKong
Senior Contributor IV

Hi Jacky, please click Correct Answer/Helpful Answer, if your question had been answered.

Thanks,

Yixing

0 Kudos
Reply

1,421 Views
max_tsai
NXP Employee
NXP Employee

hi Jacky,

Please refer to https://community.freescale.com/docs/DOC-94019

-Max