how to enable lvds split mode for uboot-2015.04

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

how to enable lvds split mode for uboot-2015.04

1,336 次查看
fulinux
Contributor IV


Hi,

i have tested uboot-2009.08 logo, but it not good(look at this thread uboot logo color is not normal ) i want to test uboot-2015.05 what it is fsl new version. for my lcd panel is 1920x1080 pix, it should use split mode, i don't know how to modify uboot-2015.04 to enable split mode, is it doesn't matter with this thread Patch to support uboot logo keep from uboot to kernel for NXP Linux and Android BSP (HDMI, LCD and L...  right ?

标签 (1)
标记 (2)
0 项奖励
回复
1 回复

871 次查看
b36401
NXP Employee
NXP Employee

You can try to configure it manually with updating LDB_CTRL register.

Please refer to 39.6.1 "LDB Control Register" chapter of i.MX 6Dual/6Quad Applications Processor Reference Manual.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复