how to display the data streams of 4 network cameras on an LCD screen via RTSP

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

how to display the data streams of 4 network cameras on an LCD screen via RTSP

1,910 次查看
Liubin2
Contributor I

        what should I do if I want to display the data streams of 4 network cameras on an LCD screen via RTSP? What are the instructions?

    The usb camera can be operated like the following, but how to operate the network camera?

gst-launch-1.0 -v imxcompositor_g2d name=comp \ sink_0::xpos=0 sink_0::ypos=0 sink_0::width=640 sink_0::height=480 \ sink_1::xpos=0 sink_1::ypos=480 sink_1::width=640 sink_1::height=480 ! \ video/x-raw,format=RGB16 ! autovideosink \ v4l2src device=/dev/video0 ! video/x-raw,width=640,height=480 ! comp.sink_0 \ v4l2src device=/dev/video1 ! video/x-raw,width=640,height=480 ! comp.sink_1

0 项奖励
回复
4 回复数

1,904 次查看
Liubin2
Contributor I

I found the following way to achieve it, but it can only display videos from three IP Camera at most,

The instructions for displaying three IP camera videos normally are as follows(it ok):

gst-launch-1.0 imxcompositor_g2d name=comp sink_0::xpos=0 sink_0::ypos=0 sink_0::width=512 sink_0::height=300 sink_1::xpos=0 sink_1::ypos=300 sink_1::width=512 sink_1::height=300 sink_2::xpos=512 sink_2::ypos=0 sink_2::width=512 sink_2::height=300 ! video/x-raw,format=RGB16 ! waylandsink rtspsrc location=rtsp://admin:cx123456@192.168.60.64 ! rtph264depay ! queue max-size-time=0 ! vpudec ! imxvideoconvert_g2d ! video/x-raw, format=RGB16, width=512, height=300 ! comp.sink_0 rtspsrc location=rtsp://admin:cx123456@192.168.60.64 ! rtph264depay ! queue max-size-time=0 ! vpudec ! imxvideoconvert_g2d ! video/x-raw, format=RGB16, width=512, height=300 ! comp.sink_1 rtspsrc location=rtsp://admin:cx123456@192.168.60.64 ! rtph264depay ! queue max-size-time=0 ! vpudec ! imxvideoconvert_g2d ! video/x-raw, format=RGB16, width=512, height=300 ! comp.sink_2

Liubin2_2-1605860255124.png

 

But when I use the command to display 4 IP camera videos, an error occurs, as shown below. What is the reason?

gst-launch-1.0 imxcompositor_g2d name=comp sink_0::xpos=0 sink_0::ypos=0 sink_0::width=512 sink_0::height=300 sink_1::xpos=0 sink_1::ypos=300 sink_1::width=512 sink_1::height=300 sink_2::xpos=512 sink_2::ypos=0 sink_2::width=512 sink_2::height=300 sink_3::xpos=512 sink_3::ypos=300 sink_3::width=512 sink_3::height=300 ! video/x-raw,format=RGB16 ! waylandsink rtspsrc location=rtsp://admin:cx123456@192.168.60.64 ! rtph264depay ! queue max-size-time=0 ! vpudec ! imxvideoconvert_g2d ! video/x-raw, format=RGB16, width=512, height=300 ! comp.sink_0 rtspsrc location=rtsp://admin:cx123456@192.168.60.64 ! rtph264depay ! queue max-size-time=0 ! vpudec ! imxvideoconvert_g2d ! video/x-raw, format=RGB16, width=512, height=300 ! comp.sink_1 rtspsrc location=rtsp://admin:cx123456@192.168.60.64 ! rtph264depay ! queue max-size-time=0 ! vpudec ! imxvideoconvert_g2d ! video/x-raw, format=RGB16, width=512, height=300 ! comp.sink_2 rtspsrc location=rtsp://admin:cx123456@192.168.60.64 ! rtph264depay ! queue max-size-time=0 ! vpudec ! imxvideoconvert_g2d ! video/x-raw, format=RGB16, width=512, height=300 ! comp.sink_3

Liubin2_0-1605860145393.png

 

 

0 项奖励
回复

1,879 次查看
joanxie
NXP TechSupport
NXP TechSupport

still 8mm board, right? what video resolution do you use? how about try the lower resolution video?

0 项奖励
回复

1,874 次查看
Liubin2
Contributor I

hi:     

      They are all 8mm boards. The current phenomenon of playing 4 videos sometimes works normally, sometimes it doesn’t work. I tried a lower resolution and it doesn’t work. Will it be related to the IP camera?

0 项奖励
回复

1,866 次查看
joanxie
NXP TechSupport
NXP TechSupport

I'm not sure if the network has issue or not? 8mm boards can support 4 rtsp video I think

0 项奖励
回复