how to disable chromium update notice to popping up?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to disable chromium update notice to popping up?

ソリューションへジャンプ
7,609件の閲覧回数
gonewithwind-peter
Senior Contributor I

Hi all,

I use imx8 maaxboad,iwave board. we use chromium  -kiosk  webpage  as user GUI(of course ,there is no menu,no settings ...(3 points ),no webpage bar....

but the  chromium  keep popping up update  notice to dispplay. how to disable it  when starting  up chromium with options or in setting config files in somewhere? (of course , can not use menu to change it manually).

I searched online, but do not find solutions  up to now.

 

any help?

 

Thank you very much.

 

0 件の賞賛
返信
1 解決策
7,559件の閲覧回数
gonewithwind-peter
Senior Contributor I

The following are the relevant flags we set. Of these, the --simulate-outdated-no-au argument is the one you need for this issue, but we specify a bunch more to suppress behaviour that assumes a user present or is otherwise desirable in a kiosk.

exec /usr/bin/chromium \
  --kiosk --enable-fullscreen \
  --touch-events=enabled \
  --activate-on-launch \
  --noerrdialogs \
  --remote-debugging-port=9222 \
  --disable-pinch \
  --disable-features=OverscrollHistoryNavigation \
  --start-maximized \
  --disable-infobars \
  --disable-notifications \
  --disable-session-crashed-bubble \
  --no-first-run \
  --enable-offline-auto-reload \
  --autoplay-policy=no-user-gesture-required \
  --deny-permission-prompts \
  --disable-search-geolocation-disclosure \
  --enable-ipv6 $CHROMIUM_EXTRAS \
  --simulate-outdated-no-au='Tue, 31 Dec 2099 23:59:59 GMT' \
  --disable-component-update \
  --allow-browser-signin=false \
  "${KIOSK_URI}"

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
7,560件の閲覧回数
gonewithwind-peter
Senior Contributor I

The following are the relevant flags we set. Of these, the --simulate-outdated-no-au argument is the one you need for this issue, but we specify a bunch more to suppress behaviour that assumes a user present or is otherwise desirable in a kiosk.

exec /usr/bin/chromium \
  --kiosk --enable-fullscreen \
  --touch-events=enabled \
  --activate-on-launch \
  --noerrdialogs \
  --remote-debugging-port=9222 \
  --disable-pinch \
  --disable-features=OverscrollHistoryNavigation \
  --start-maximized \
  --disable-infobars \
  --disable-notifications \
  --disable-session-crashed-bubble \
  --no-first-run \
  --enable-offline-auto-reload \
  --autoplay-policy=no-user-gesture-required \
  --deny-permission-prompts \
  --disable-search-geolocation-disclosure \
  --enable-ipv6 $CHROMIUM_EXTRAS \
  --simulate-outdated-no-au='Tue, 31 Dec 2099 23:59:59 GMT' \
  --disable-component-update \
  --allow-browser-signin=false \
  "${KIOSK_URI}"

0 件の賞賛
返信
7,586件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

@gonewithwind-peter 

 

Did you try add this :–disable-desktop-notifications ?

0 件の賞賛
返信
7,569件の閲覧回数
gonewithwind-peter
Senior Contributor I

@Zhiming_Liu 

I add that option, but not work.

 

 

can I remove the message from the source code?

I find the message at file :

./tmp-glibc/work/aarch64-oe-linux/chromium-x11/76.0.3809.100-r0/chromium-76.0.3809.100/chrome/app/chromium_strings.grd

but I not not sure how to remove it.

 

anybody any help?

 

 

0 件の賞賛
返信
7,579件の閲覧回数
gonewithwind-peter
Senior Contributor I

@Zhiming_Liu 

let me try to add it , thanks

0 件の賞賛
返信