how to disable 3D engine on i.mx6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

how to disable 3D engine on i.mx6

2,961 次查看
ryanschroeder
NXP Employee
NXP Employee

we're battling thermal issues in our i.MX6 design. The i.MX6 will exceed 95°C at 70°C ambient.

We were told that the 3D engine could be disabled in our system and that should reduce the core temperature of the i.MX6. I am not sure what actually controls the power of the 3D engine....is it the kernel, video codec, gstreamer, Qt?

Can someone please provide any information on how to disable the 3D engine (if this is even possible)?

标签 (1)
0 项奖励
回复
1 回复

2,478 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ryan

one can remove gpu drivers from linux build, please refer to

attached Linux Manual sect.13.1.1.6 Menu Configuration Options

or use core-image-minimal, base as in Yocto Guide Table 1. Freescale

Yocto project images. In running image (if nobody uses gpu)

one can disable its clocks in CCM_CCGR1 and gate LDO_PU regulator

using register PMU_REG_CORE[REG1_TARG], note it also powers vpu

module. Also it may be useful to look at

Imx6q:How to caribrate cpu temp, modify thermal configuration?

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复