how to default use a72 instead of a53 with imx8qm

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to default use a72 instead of a53 with imx8qm

ソリューションへジャンプ
4,979件の閲覧回数
jiangyaqiang
Contributor V

HI :

       Currecntly, when boot up MEK board of imx8qm, the default cpu cpu0 is a53, does there any way to change to a72 ?

0 件の賞賛
返信
1 解決策
4,879件の閲覧回数
zhao_yang
NXP Employee
NXP Employee

OK, The following picture  is the detail information about the doc.

pastedImage_1.png

I also add the  attachments here.

元の投稿で解決策を見る

0 件の賞賛
返信
7 返答(返信)
4,879件の閲覧回数
zhao_yang
NXP Employee
NXP Employee

hi,Yaqiang

Here is an example to change the primary CPU as A72. I hope this can give you some help.

https://community.nxp.com/docs/DOC-347300 

0 件の賞賛
返信
4,879件の閲覧回数
jiangyaqiang
Contributor V

HI Zhao:

Thanks, but I can't access the link:

pastedImage_1.png

0 件の賞賛
返信
4,880件の閲覧回数
zhao_yang
NXP Employee
NXP Employee

OK, The following picture  is the detail information about the doc.

pastedImage_1.png

I also add the  attachments here.

0 件の賞賛
返信
3,272件の閲覧回数
aroffelsen
Contributor I

What are these patches supposed to be applied to?

0 件の賞賛
返信
4,809件の閲覧回数
传策薛
Contributor V

I use the Android9.0

0 件の賞賛
返信
4,815件の閲覧回数
传策薛
Contributor V

Hi, how to patch "A53-to-A72-trusty-001.patch"

0 件の賞賛
返信
4,879件の閲覧回数
lily_zhang
NXP Employee
NXP Employee

zhaoyang-b49593‌, please help on it.

0 件の賞賛
返信