how to default use a72 instead of a53 with imx8qm

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to default use a72 instead of a53 with imx8qm

Jump to solution
5,006 Views
jiangyaqiang
Contributor V

HI :

       Currecntly, when boot up MEK board of imx8qm, the default cpu cpu0 is a53, does there any way to change to a72 ?

0 Kudos
Reply
1 Solution
4,906 Views
zhao_yang
NXP Employee
NXP Employee

OK, The following picture  is the detail information about the doc.

pastedImage_1.png

I also add the  attachments here.

View solution in original post

0 Kudos
Reply
7 Replies
4,906 Views
zhao_yang
NXP Employee
NXP Employee

hi,Yaqiang

Here is an example to change the primary CPU as A72. I hope this can give you some help.

https://community.nxp.com/docs/DOC-347300 

0 Kudos
Reply
4,906 Views
jiangyaqiang
Contributor V

HI Zhao:

Thanks, but I can't access the link:

pastedImage_1.png

0 Kudos
Reply
4,907 Views
zhao_yang
NXP Employee
NXP Employee

OK, The following picture  is the detail information about the doc.

pastedImage_1.png

I also add the  attachments here.

0 Kudos
Reply
3,299 Views
aroffelsen
Contributor I

What are these patches supposed to be applied to?

0 Kudos
Reply
4,836 Views
传策薛
Contributor V

I use the Android9.0

0 Kudos
Reply
4,842 Views
传策薛
Contributor V

Hi, how to patch "A53-to-A72-trusty-001.patch"

0 Kudos
Reply
4,906 Views
lily_zhang
NXP Employee
NXP Employee

zhaoyang-b49593‌, please help on it.

0 Kudos
Reply