how to change ddr to 2G on u-boot 2015.04

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to change ddr to 2G on u-boot 2015.04

ソリューションへジャンプ
6,061件の閲覧回数
tootzoe
Contributor III

Hi all,

I built   Android 5.1.1 on imx6q-sabre SD, my custom board uses 2G DRAM, u-boot is Version 2015.04 , I had test my ddr with  i.MX6/7 DDR Stress Test Tool V2.40 and got the calibration result,  now I need to apply this change into u-boot, otherwise my custom board can't run correctly,  i found  u-boot source code is different from the version before,  I have search the whole community for how to modify the new u-boot, but without lucky.

could somebody help chage DRAM from 1G to 2G on u-boot 2015.04?

Best regards

toot

ラベル(1)
1 解決策
3,868件の閲覧回数
tootzoe
Contributor III

i followed this post:

i.Mx6DQSDL DDR3 Script Aid

change the DRAM parameter  on my custom board, 4 piece k4b4g1646d  DRAM (total 2G bytes) run very well,

here is the calibration result:

============================================

        DDR Stress Test (2.4.0)

        Build: Dec 11 2015, 11:13:38

        Freescale Semiconductor, Inc.

============================================

============================================

        Chip ID

CHIP ID = i.MX6 Dual/Quad (0x63)

Internal Revision = TO1.5

============================================

============================================

        Boot Configuration

SRC_SBMR1(0x020d8004) = 0x00000000

SRC_SBMR2(0x020d801c) = 0x22000001

============================================

ARM Clock set to 1GHz

============================================

        DDR configuration

BOOT_CFG3[5-4]: 0x00, Single DDR channel.

DDR type is DDR3

Data width: 64, bank num: 8

Row size: 15, col size: 10

Chip select CSD0 is used

Density per chip select: 2048MB

============================================

Current Tempareture: 49

============================================

DDR Freq: 528 MHz

ddr_mr1=0x00000000

Start write leveling calibration...

running Write level HW calibration

Write leveling calibration completed, update the following registers in your initialization script

    MMDC_MPWLDECTRL0 ch0 (0x021b080c) = 0x00260022

    MMDC_MPWLDECTRL1 ch0 (0x021b0810) = 0x002B002B

    MMDC_MPWLDECTRL0 ch1 (0x021b480c) = 0x001D0028

    MMDC_MPWLDECTRL1 ch1 (0x021b4810) = 0x000D0028

Write DQS delay result:

   Write DQS0 delay: 34/256 CK

   Write DQS1 delay: 38/256 CK

   Write DQS2 delay: 43/256 CK

   Write DQS3 delay: 43/256 CK

   Write DQS4 delay: 40/256 CK

   Write DQS5 delay: 29/256 CK

   Write DQS6 delay: 40/256 CK

   Write DQS7 delay: 13/256 CK

Starting DQS gating calibration

. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . .

. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . .

BYTE 0:

  Start: HC=0x01 ABS=0x70

  End: HC=0x04 ABS=0x34

  Mean: HC=0x03 ABS=0x12

  End-0.5*tCK: HC=0x03 ABS=0x34

  Final: HC=0x03 ABS=0x34

BYTE 1:

  Start: HC=0x01 ABS=0x4C

  End: HC=0x04 ABS=0x28

  Mean: HC=0x02 ABS=0x79

  End-0.5*tCK: HC=0x03 ABS=0x28

  Final: HC=0x03 ABS=0x28

BYTE 2:

  Start: HC=0x01 ABS=0x54

  End: HC=0x04 ABS=0x14

  Mean: HC=0x02 ABS=0x73

  End-0.5*tCK: HC=0x03 ABS=0x14

  Final: HC=0x03 ABS=0x14

BYTE 3:

  Start: HC=0x00 ABS=0x4C

  End: HC=0x04 ABS=0x1C

  Mean: HC=0x02 ABS=0x34

  End-0.5*tCK: HC=0x03 ABS=0x1C

  Final: HC=0x03 ABS=0x1C

BYTE 4:

  Start: HC=0x01 ABS=0x60

  End: HC=0x04 ABS=0x34

  Mean: HC=0x03 ABS=0x0A

  End-0.5*tCK: HC=0x03 ABS=0x34

  Final: HC=0x03 ABS=0x34

BYTE 5:

  Start: HC=0x01 ABS=0x60

  End: HC=0x04 ABS=0x24

  Mean: HC=0x03 ABS=0x02

  End-0.5*tCK: HC=0x03 ABS=0x24

  Final: HC=0x03 ABS=0x24

BYTE 6:

  Start: HC=0x01 ABS=0x38

  End: HC=0x03 ABS=0x5C

  Mean: HC=0x02 ABS=0x4A

  End-0.5*tCK: HC=0x02 ABS=0x5C

  Final: HC=0x02 ABS=0x5C

BYTE 7:

  Start: HC=0x01 ABS=0x58

  End: HC=0x04 ABS=0x1C

  Mean: HC=0x02 ABS=0x79

  End-0.5*tCK: HC=0x03 ABS=0x1C

  Final: HC=0x03 ABS=0x1C

DQS calibration MMDC0 MPDGCTRL0 = 0x03280334, MPDGCTRL1 = 0x031C0314

DQS calibration MMDC1 MPDGCTRL0 = 0x03240334, MPDGCTRL1 = 0x031C025C

Note: Array result[] holds the DRAM test result of each byte. 

      0: test pass.  1: test fail 

      4 bits respresent the result of 1 byte.   

      result 00000001:byte 0 fail.

      result 00000011:byte 0, 1 fail.

Starting Read calibration...

ABS_OFFSET=0x00000000 result[00]=0x11111111

ABS_OFFSET=0x04040404 result[01]=0x11111111

ABS_OFFSET=0x08080808 result[02]=0x11111111

ABS_OFFSET=0x0C0C0C0C result[03]=0x11111111

ABS_OFFSET=0x10101010 result[04]=0x00011011

ABS_OFFSET=0x14141414 result[05]=0x00011011

ABS_OFFSET=0x18181818 result[06]=0x00011001

ABS_OFFSET=0x1C1C1C1C result[07]=0x00011000

ABS_OFFSET=0x20202020 result[08]=0x00000000

ABS_OFFSET=0x24242424 result[09]=0x00000000

ABS_OFFSET=0x28282828 result[0A]=0x00000000

ABS_OFFSET=0x2C2C2C2C result[0B]=0x00000000

ABS_OFFSET=0x30303030 result[0C]=0x00000000

ABS_OFFSET=0x34343434 result[0D]=0x00000000

ABS_OFFSET=0x38383838 result[0E]=0x00000000

ABS_OFFSET=0x3C3C3C3C result[0F]=0x00000000

ABS_OFFSET=0x40404040 result[10]=0x00000000

ABS_OFFSET=0x44444444 result[11]=0x00000000

ABS_OFFSET=0x48484848 result[12]=0x00000000

ABS_OFFSET=0x4C4C4C4C result[13]=0x00000000

ABS_OFFSET=0x50505050 result[14]=0x00000000

ABS_OFFSET=0x54545454 result[15]=0x00000000

ABS_OFFSET=0x58585858 result[16]=0x00000000

ABS_OFFSET=0x5C5C5C5C result[17]=0x00000000

ABS_OFFSET=0x60606060 result[18]=0x01100010

ABS_OFFSET=0x64646464 result[19]=0x01100111

ABS_OFFSET=0x68686868 result[1A]=0x01100111

ABS_OFFSET=0x6C6C6C6C result[1B]=0x11100111

ABS_OFFSET=0x70707070 result[1C]=0x11100111

ABS_OFFSET=0x74747474 result[1D]=0x11111111

ABS_OFFSET=0x78787878 result[1E]=0x11111111

ABS_OFFSET=0x7C7C7C7C result[1F]=0x11111111

Byte 0: (0x1c - 0x60), middle value:0x3e

Byte 1: (0x18 - 0x5c), middle value:0x3a

Byte 2: (0x10 - 0x60), middle value:0x38

Byte 3: (0x20 - 0x70), middle value:0x48

Byte 4: (0x20 - 0x70), middle value:0x48

Byte 5: (0x10 - 0x5c), middle value:0x36

Byte 6: (0x10 - 0x5c), middle value:0x36

Byte 7: (0x10 - 0x68), middle value:0x3c

MMDC0 MPRDDLCTL = 0x48383A3E, MMDC1 MPRDDLCTL = 0x3C363648

Starting Write calibration...

ABS_OFFSET=0x00000000 result[00]=0x11111111

ABS_OFFSET=0x04040404 result[01]=0x10111111

ABS_OFFSET=0x08080808 result[02]=0x10111111

ABS_OFFSET=0x0C0C0C0C result[03]=0x10110111

ABS_OFFSET=0x10101010 result[04]=0x10100011

ABS_OFFSET=0x14141414 result[05]=0x10100010

ABS_OFFSET=0x18181818 result[06]=0x00100000

ABS_OFFSET=0x1C1C1C1C result[07]=0x00100000

ABS_OFFSET=0x20202020 result[08]=0x00000000

ABS_OFFSET=0x24242424 result[09]=0x00000000

ABS_OFFSET=0x28282828 result[0A]=0x00000000

ABS_OFFSET=0x2C2C2C2C result[0B]=0x00000000

ABS_OFFSET=0x30303030 result[0C]=0x00000000

ABS_OFFSET=0x34343434 result[0D]=0x00000000

ABS_OFFSET=0x38383838 result[0E]=0x00000000

ABS_OFFSET=0x3C3C3C3C result[0F]=0x00000000

ABS_OFFSET=0x40404040 result[10]=0x00000000

ABS_OFFSET=0x44444444 result[11]=0x00000000

ABS_OFFSET=0x48484848 result[12]=0x00000000

ABS_OFFSET=0x4C4C4C4C result[13]=0x00000000

ABS_OFFSET=0x50505050 result[14]=0x00000000

ABS_OFFSET=0x54545454 result[15]=0x00000000

ABS_OFFSET=0x58585858 result[16]=0x00000000

ABS_OFFSET=0x5C5C5C5C result[17]=0x00000000

ABS_OFFSET=0x60606060 result[18]=0x00000000

ABS_OFFSET=0x64646464 result[19]=0x00000000

ABS_OFFSET=0x68686868 result[1A]=0x00001000

ABS_OFFSET=0x6C6C6C6C result[1B]=0x01001000

ABS_OFFSET=0x70707070 result[1C]=0x01001110

ABS_OFFSET=0x74747474 result[1D]=0x01011111

ABS_OFFSET=0x78787878 result[1E]=0x01011111

ABS_OFFSET=0x7C7C7C7C result[1F]=0x11111111

Byte 0: (0x14 - 0x70), middle value:0x42

Byte 1: (0x18 - 0x6c), middle value:0x42

Byte 2: (0x10 - 0x6c), middle value:0x3e

Byte 3: (0x0c - 0x64), middle value:0x38

Byte 4: (0x10 - 0x70), middle value:0x40

Byte 5: (0x20 - 0x78), middle value:0x4c

Byte 6: (0x04 - 0x68), middle value:0x36

Byte 7: (0x18 - 0x78), middle value:0x48

MMDC0 MPWRDLCTL = 0x383E4242,MMDC1 MPWRDLCTL = 0x48364C40

   MMDC registers updated from calibration

   Write leveling calibration

   MMDC_MPWLDECTRL0 ch0 (0x021b080c) = 0x00260022

   MMDC_MPWLDECTRL1 ch0 (0x021b0810) = 0x002B002B

   MMDC_MPWLDECTRL0 ch1 (0x021b480c) = 0x001D0028

   MMDC_MPWLDECTRL1 ch1 (0x021b4810) = 0x000D0028

   Read DQS Gating calibration

   MPDGCTRL0 PHY0 (0x021b083c) = 0x03280334

   MPDGCTRL1 PHY0 (0x021b0840) = 0x031C0314

   MPDGCTRL0 PHY1 (0x021b483c) = 0x03240334

   MPDGCTRL1 PHY1 (0x021b4840) = 0x031C025C

   Read calibration

   MPRDDLCTL PHY0 (0x021b0848) = 0x48383A3E

   MPRDDLCTL PHY1 (0x021b4848) = 0x3C363648

   Write calibration

   MPWRDLCTL PHY0 (0x021b0850) = 0x383E4242

   MPWRDLCTL PHY1 (0x021b4850) = 0x48364C40

Success: DDR calibration completed!!!

  

Device Information
Manufacturer:samsung
Memory part number:k4b4g1646d
Memory type:DDR3-1600
DRAM density (Gb)4
DRAM Bus Width16
Number of Banks8
Number of ROW Addresses15
Number of COLUMN Addresses10
Page Size (K)2
Self-Refresh Temperature (SRT)Normal
tRCD=tRP=CL (ns)13.75
tRC Min (ns)48.75
tRAS Min (ns)35
System Information
i.Mx Parti.Mx6Q
Bus Width64
Density per chip select (Gb)16
Number of Chip Selects used1
Total DRAM Density (Gb)16
DRAM Clock Freq (MHz)528
DRAM Clock Cycle Time (ns)1.894
Address Mirror (for CS1)Disable
SI Configuration
DRAM DSE Setting - DQ/DQM (ohm)48
DRAM DSE Setting - ADDR/CMD/CTL (ohm)48
DRAM DSE Setting - CK (ohm)48
DRAM DSE Setting - DQS (ohm)48
System ODT Setting (ohm)60

元の投稿で解決策を見る

6 返答(返信)
3,869件の閲覧回数
tootzoe
Contributor III

i followed this post:

i.Mx6DQSDL DDR3 Script Aid

change the DRAM parameter  on my custom board, 4 piece k4b4g1646d  DRAM (total 2G bytes) run very well,

here is the calibration result:

============================================

        DDR Stress Test (2.4.0)

        Build: Dec 11 2015, 11:13:38

        Freescale Semiconductor, Inc.

============================================

============================================

        Chip ID

CHIP ID = i.MX6 Dual/Quad (0x63)

Internal Revision = TO1.5

============================================

============================================

        Boot Configuration

SRC_SBMR1(0x020d8004) = 0x00000000

SRC_SBMR2(0x020d801c) = 0x22000001

============================================

ARM Clock set to 1GHz

============================================

        DDR configuration

BOOT_CFG3[5-4]: 0x00, Single DDR channel.

DDR type is DDR3

Data width: 64, bank num: 8

Row size: 15, col size: 10

Chip select CSD0 is used

Density per chip select: 2048MB

============================================

Current Tempareture: 49

============================================

DDR Freq: 528 MHz

ddr_mr1=0x00000000

Start write leveling calibration...

running Write level HW calibration

Write leveling calibration completed, update the following registers in your initialization script

    MMDC_MPWLDECTRL0 ch0 (0x021b080c) = 0x00260022

    MMDC_MPWLDECTRL1 ch0 (0x021b0810) = 0x002B002B

    MMDC_MPWLDECTRL0 ch1 (0x021b480c) = 0x001D0028

    MMDC_MPWLDECTRL1 ch1 (0x021b4810) = 0x000D0028

Write DQS delay result:

   Write DQS0 delay: 34/256 CK

   Write DQS1 delay: 38/256 CK

   Write DQS2 delay: 43/256 CK

   Write DQS3 delay: 43/256 CK

   Write DQS4 delay: 40/256 CK

   Write DQS5 delay: 29/256 CK

   Write DQS6 delay: 40/256 CK

   Write DQS7 delay: 13/256 CK

Starting DQS gating calibration

. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . .

. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . .

BYTE 0:

  Start: HC=0x01 ABS=0x70

  End: HC=0x04 ABS=0x34

  Mean: HC=0x03 ABS=0x12

  End-0.5*tCK: HC=0x03 ABS=0x34

  Final: HC=0x03 ABS=0x34

BYTE 1:

  Start: HC=0x01 ABS=0x4C

  End: HC=0x04 ABS=0x28

  Mean: HC=0x02 ABS=0x79

  End-0.5*tCK: HC=0x03 ABS=0x28

  Final: HC=0x03 ABS=0x28

BYTE 2:

  Start: HC=0x01 ABS=0x54

  End: HC=0x04 ABS=0x14

  Mean: HC=0x02 ABS=0x73

  End-0.5*tCK: HC=0x03 ABS=0x14

  Final: HC=0x03 ABS=0x14

BYTE 3:

  Start: HC=0x00 ABS=0x4C

  End: HC=0x04 ABS=0x1C

  Mean: HC=0x02 ABS=0x34

  End-0.5*tCK: HC=0x03 ABS=0x1C

  Final: HC=0x03 ABS=0x1C

BYTE 4:

  Start: HC=0x01 ABS=0x60

  End: HC=0x04 ABS=0x34

  Mean: HC=0x03 ABS=0x0A

  End-0.5*tCK: HC=0x03 ABS=0x34

  Final: HC=0x03 ABS=0x34

BYTE 5:

  Start: HC=0x01 ABS=0x60

  End: HC=0x04 ABS=0x24

  Mean: HC=0x03 ABS=0x02

  End-0.5*tCK: HC=0x03 ABS=0x24

  Final: HC=0x03 ABS=0x24

BYTE 6:

  Start: HC=0x01 ABS=0x38

  End: HC=0x03 ABS=0x5C

  Mean: HC=0x02 ABS=0x4A

  End-0.5*tCK: HC=0x02 ABS=0x5C

  Final: HC=0x02 ABS=0x5C

BYTE 7:

  Start: HC=0x01 ABS=0x58

  End: HC=0x04 ABS=0x1C

  Mean: HC=0x02 ABS=0x79

  End-0.5*tCK: HC=0x03 ABS=0x1C

  Final: HC=0x03 ABS=0x1C

DQS calibration MMDC0 MPDGCTRL0 = 0x03280334, MPDGCTRL1 = 0x031C0314

DQS calibration MMDC1 MPDGCTRL0 = 0x03240334, MPDGCTRL1 = 0x031C025C

Note: Array result[] holds the DRAM test result of each byte. 

      0: test pass.  1: test fail 

      4 bits respresent the result of 1 byte.   

      result 00000001:byte 0 fail.

      result 00000011:byte 0, 1 fail.

Starting Read calibration...

ABS_OFFSET=0x00000000 result[00]=0x11111111

ABS_OFFSET=0x04040404 result[01]=0x11111111

ABS_OFFSET=0x08080808 result[02]=0x11111111

ABS_OFFSET=0x0C0C0C0C result[03]=0x11111111

ABS_OFFSET=0x10101010 result[04]=0x00011011

ABS_OFFSET=0x14141414 result[05]=0x00011011

ABS_OFFSET=0x18181818 result[06]=0x00011001

ABS_OFFSET=0x1C1C1C1C result[07]=0x00011000

ABS_OFFSET=0x20202020 result[08]=0x00000000

ABS_OFFSET=0x24242424 result[09]=0x00000000

ABS_OFFSET=0x28282828 result[0A]=0x00000000

ABS_OFFSET=0x2C2C2C2C result[0B]=0x00000000

ABS_OFFSET=0x30303030 result[0C]=0x00000000

ABS_OFFSET=0x34343434 result[0D]=0x00000000

ABS_OFFSET=0x38383838 result[0E]=0x00000000

ABS_OFFSET=0x3C3C3C3C result[0F]=0x00000000

ABS_OFFSET=0x40404040 result[10]=0x00000000

ABS_OFFSET=0x44444444 result[11]=0x00000000

ABS_OFFSET=0x48484848 result[12]=0x00000000

ABS_OFFSET=0x4C4C4C4C result[13]=0x00000000

ABS_OFFSET=0x50505050 result[14]=0x00000000

ABS_OFFSET=0x54545454 result[15]=0x00000000

ABS_OFFSET=0x58585858 result[16]=0x00000000

ABS_OFFSET=0x5C5C5C5C result[17]=0x00000000

ABS_OFFSET=0x60606060 result[18]=0x01100010

ABS_OFFSET=0x64646464 result[19]=0x01100111

ABS_OFFSET=0x68686868 result[1A]=0x01100111

ABS_OFFSET=0x6C6C6C6C result[1B]=0x11100111

ABS_OFFSET=0x70707070 result[1C]=0x11100111

ABS_OFFSET=0x74747474 result[1D]=0x11111111

ABS_OFFSET=0x78787878 result[1E]=0x11111111

ABS_OFFSET=0x7C7C7C7C result[1F]=0x11111111

Byte 0: (0x1c - 0x60), middle value:0x3e

Byte 1: (0x18 - 0x5c), middle value:0x3a

Byte 2: (0x10 - 0x60), middle value:0x38

Byte 3: (0x20 - 0x70), middle value:0x48

Byte 4: (0x20 - 0x70), middle value:0x48

Byte 5: (0x10 - 0x5c), middle value:0x36

Byte 6: (0x10 - 0x5c), middle value:0x36

Byte 7: (0x10 - 0x68), middle value:0x3c

MMDC0 MPRDDLCTL = 0x48383A3E, MMDC1 MPRDDLCTL = 0x3C363648

Starting Write calibration...

ABS_OFFSET=0x00000000 result[00]=0x11111111

ABS_OFFSET=0x04040404 result[01]=0x10111111

ABS_OFFSET=0x08080808 result[02]=0x10111111

ABS_OFFSET=0x0C0C0C0C result[03]=0x10110111

ABS_OFFSET=0x10101010 result[04]=0x10100011

ABS_OFFSET=0x14141414 result[05]=0x10100010

ABS_OFFSET=0x18181818 result[06]=0x00100000

ABS_OFFSET=0x1C1C1C1C result[07]=0x00100000

ABS_OFFSET=0x20202020 result[08]=0x00000000

ABS_OFFSET=0x24242424 result[09]=0x00000000

ABS_OFFSET=0x28282828 result[0A]=0x00000000

ABS_OFFSET=0x2C2C2C2C result[0B]=0x00000000

ABS_OFFSET=0x30303030 result[0C]=0x00000000

ABS_OFFSET=0x34343434 result[0D]=0x00000000

ABS_OFFSET=0x38383838 result[0E]=0x00000000

ABS_OFFSET=0x3C3C3C3C result[0F]=0x00000000

ABS_OFFSET=0x40404040 result[10]=0x00000000

ABS_OFFSET=0x44444444 result[11]=0x00000000

ABS_OFFSET=0x48484848 result[12]=0x00000000

ABS_OFFSET=0x4C4C4C4C result[13]=0x00000000

ABS_OFFSET=0x50505050 result[14]=0x00000000

ABS_OFFSET=0x54545454 result[15]=0x00000000

ABS_OFFSET=0x58585858 result[16]=0x00000000

ABS_OFFSET=0x5C5C5C5C result[17]=0x00000000

ABS_OFFSET=0x60606060 result[18]=0x00000000

ABS_OFFSET=0x64646464 result[19]=0x00000000

ABS_OFFSET=0x68686868 result[1A]=0x00001000

ABS_OFFSET=0x6C6C6C6C result[1B]=0x01001000

ABS_OFFSET=0x70707070 result[1C]=0x01001110

ABS_OFFSET=0x74747474 result[1D]=0x01011111

ABS_OFFSET=0x78787878 result[1E]=0x01011111

ABS_OFFSET=0x7C7C7C7C result[1F]=0x11111111

Byte 0: (0x14 - 0x70), middle value:0x42

Byte 1: (0x18 - 0x6c), middle value:0x42

Byte 2: (0x10 - 0x6c), middle value:0x3e

Byte 3: (0x0c - 0x64), middle value:0x38

Byte 4: (0x10 - 0x70), middle value:0x40

Byte 5: (0x20 - 0x78), middle value:0x4c

Byte 6: (0x04 - 0x68), middle value:0x36

Byte 7: (0x18 - 0x78), middle value:0x48

MMDC0 MPWRDLCTL = 0x383E4242,MMDC1 MPWRDLCTL = 0x48364C40

   MMDC registers updated from calibration

   Write leveling calibration

   MMDC_MPWLDECTRL0 ch0 (0x021b080c) = 0x00260022

   MMDC_MPWLDECTRL1 ch0 (0x021b0810) = 0x002B002B

   MMDC_MPWLDECTRL0 ch1 (0x021b480c) = 0x001D0028

   MMDC_MPWLDECTRL1 ch1 (0x021b4810) = 0x000D0028

   Read DQS Gating calibration

   MPDGCTRL0 PHY0 (0x021b083c) = 0x03280334

   MPDGCTRL1 PHY0 (0x021b0840) = 0x031C0314

   MPDGCTRL0 PHY1 (0x021b483c) = 0x03240334

   MPDGCTRL1 PHY1 (0x021b4840) = 0x031C025C

   Read calibration

   MPRDDLCTL PHY0 (0x021b0848) = 0x48383A3E

   MPRDDLCTL PHY1 (0x021b4848) = 0x3C363648

   Write calibration

   MPWRDLCTL PHY0 (0x021b0850) = 0x383E4242

   MPWRDLCTL PHY1 (0x021b4850) = 0x48364C40

Success: DDR calibration completed!!!

  

Device Information
Manufacturer:samsung
Memory part number:k4b4g1646d
Memory type:DDR3-1600
DRAM density (Gb)4
DRAM Bus Width16
Number of Banks8
Number of ROW Addresses15
Number of COLUMN Addresses10
Page Size (K)2
Self-Refresh Temperature (SRT)Normal
tRCD=tRP=CL (ns)13.75
tRC Min (ns)48.75
tRAS Min (ns)35
System Information
i.Mx Parti.Mx6Q
Bus Width64
Density per chip select (Gb)16
Number of Chip Selects used1
Total DRAM Density (Gb)16
DRAM Clock Freq (MHz)528
DRAM Clock Cycle Time (ns)1.894
Address Mirror (for CS1)Disable
SI Configuration
DRAM DSE Setting - DQ/DQM (ohm)48
DRAM DSE Setting - ADDR/CMD/CTL (ohm)48
DRAM DSE Setting - CK (ohm)48
DRAM DSE Setting - DQS (ohm)48
System ODT Setting (ohm)60
3,868件の閲覧回数
skrait
Contributor I

I also met you in this case, how do you deal with

0 件の賞賛
返信
3,866件の閲覧回数
art
NXP Employee
NXP Employee

Please refer to the Chapter 1 of the attached document. This document can also be found as the part of the L3.14.52_1.1.0_LINUX_DOCS bundle, available on the public NXP web site (check the "Supporting Information" section):

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,865件の閲覧回数
tootzoe
Contributor III

Hi artur ,

  Thanks for replying,  according to L3.14.52_1.1.0_LINUX_DOCS Chapter 1,  I modify the register's value as following:

MMDC registers updated from calibration

  Write leveling calibration

  MMDC_MPWLDECTRL0 ch0 (0x021b080c) = 0x0022001D

  MMDC_MPWLDECTRL1 ch0 (0x021b0810) = 0x00260028

  MMDC_MPWLDECTRL0 ch1 (0x021b480c) = 0x001F0028

  MMDC_MPWLDECTRL1 ch1 (0x021b4810) = 0x00150028

  Read DQS Gating calibration

  MPDGCTRL0 PHY0 (0x021b083c) = 0x431C0330

  MPDGCTRL1 PHY0 (0x021b0840) = 0x03140314

  MPDGCTRL0 PHY1 (0x021b483c) = 0x43240334

  MPDGCTRL1 PHY1 (0x021b4840) = 0x03180258

  Read calibration

  MPRDDLCTL PHY0 (0x021b0848) = 0x4232383A

  MPRDDLCTL PHY1 (0x021b4848) = 0x38363444

  Write calibration

  MPWRDLCTL PHY0 (0x021b0850) = 0x3A3A3E3C

  MPWRDLCTL PHY1 (0x021b4850) = 0x46344842

then I recompile u-boot and boot my board with this cmd:

    > sb_loader.exe -f u-boot-imx6q.imx

the u-boot start-up message still showing my board is  DRAM:  1 GiB

could you tell me where to change the DRAM parameter ?

I attached my DDR calibration result below.

best regards

toot

0 件の賞賛
返信
3,865件の閲覧回数
art
NXP Employee
NXP Employee

Refer to the Section 1.2.1 "Preparing the Code" of the document I've sent to you. Pay attention to the configuration parameters, such as PHYS_SDRAM_SIZE and CONFIG_NR_DRAM_BANKS.

Best Regards,

Artur

0 件の賞賛
返信
3,865件の閲覧回数
tootzoe
Contributor III

Hi artur ,

i have configs as following;

#defined CONFIG_NR_DRAM_BANKS      1

#define PHYS_SDRAM_SIZE    SZ_2G

#define PHYS_SDRAM              MMDC0_ARB_BASE_ADDR             ( MMDC0_ARB_BASE_ADDR = 0x10000000  defined in arch/arm/include/asm/arch-mx6/imx-regs.h )

but u-boot still show me 1G DRAM ,   could you tell me how to config this marcos ?

best regards

toot

0 件の賞賛
返信