how to build booting from NAND flash on i.mx28evk

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

how to build booting from NAND flash on i.mx28evk

1,023 次查看
edwintu
Contributor I

Hi,

I am working on i.MX28 evk board with Linux 2.6.32 running on it. I was able to boot from SD card as instructed by doc , I use ./sdimage tp programming imx_ivt_uboot.sd in SD card, when power up, under the u-boot environment, I was able to  use tftpboot to transfer file onto the RAM of evk  and I trying to implement booting process from NAND flash, together with  kernel and rootfs,  I plan to use u-boot command ";nand erase & write" to flahing image in nand, but there is no such command support, I was wondering how I can use a NAND flash to boot up system . If yes, where can I find related procedure? or is there any other way to do for nand booting .

any advice is welcome.

Thank you in advance.

edwin

标签 (1)
标记 (1)
0 项奖励
回复
0 回复数