how to attach IVT header in imx-uboot for lollipop 5.0.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to attach IVT header in imx-uboot for lollipop 5.0.0

963 Views
vivektol
Contributor I

Hi,

I am tryping to port lollipop 5.0.0. on my custom board with imx6dl processor. emmc is connected to sd4.

After porting the images on the board, the uboot is also not getting on. On the same boards Kitkat 4.4.2 is working.

Some where I read that for lollipop we need to add IVT header to uboot. How to do it.

Please guide.

Thanks and Regards,

VIVEK TOL

Labels (4)
0 Kudos
Reply
1 Reply

792 Views
igorpadykov
NXP Employee
NXP Employee

Hi VIVEK

IVT header is generated by uboot, for new board/ddr please run ddr test

i.MX6/7 DDR Stress Test Tool V2.52 | NXP Community

and modify  uboot *.cgf file, like uboot../mx6sabresd/mx6dl_4x_mt41j128.cfg

with new calibration settings obtained from ddr test.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply