how can i use can bus with mx8 family processor ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how can i use can bus with mx8 family processor ?

1,119 Views
dogancanyuksel_
Contributor I

i did not find in datasheet ? i need harware can bus but also i can use software part.

Is mx8 quad core processor has bus protocol is not it?

0 Kudos
Reply
1 Reply

1,050 Views
igorpadykov
NXP Employee
NXP Employee

Hi dogancan

yes i.MX8QM has can module, one can look in linux documentation and try unit tests

Alpha / Beta BSPs for Microprocessors|NXP 

doc\can\test - imx-test - i.MX Driver Test Application Software 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply