how can i use can bus with mx8 family processor ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

how can i use can bus with mx8 family processor ?

1,158 次查看
dogancanyuksel_
Contributor I

i did not find in datasheet ? i need harware can bus but also i can use software part.

Is mx8 quad core processor has bus protocol is not it?

0 项奖励
回复
1 回复

1,089 次查看
igorpadykov
NXP Employee
NXP Employee

Hi dogancan

yes i.MX8QM has can module, one can look in linux documentation and try unit tests

Alpha / Beta BSPs for Microprocessors|NXP 

doc\can\test - imx-test - i.MX Driver Test Application Software 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复