how can i get imx-3.14.28-1.0.0_ga

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

how can i get imx-3.14.28-1.0.0_ga

跳至解决方案
6,568 次查看
kikimorisato
Contributor II

mkdir fsl-release-bsp-sane

cd fsl-release-bsp-sane

repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-3.14.28-1.0.0_ga

repo sync

but i can not get 3.14.28

linux.png

how can i get linux-3.14.28 ????

------------------------------------------------------------------------------------------------------------------------------------------------------------------

here is fsl-community-bsp

linux2.png

it is linux-3.14.28

标签 (3)
0 项奖励
回复
1 解答
3,258 次查看
Yuri
NXP Employee
NXP Employee

Freescale BSP Release options are located in "meta-fsl-bsp-release" directory.

Regards,

Yuri

在原帖中查看解决方案

0 项奖励
回复
6 回复数
3,258 次查看
Yuri
NXP Employee
NXP Employee

  "When this process is completed, the source code is checked out into

the directory fsl-release-bsp[-sane]/sources".


Are there error messages ?


If you have an HTTPS proxy and your firewall supports socks, section  2 (How

do I download the Android source code behind a firewall?) of Android documentation

helps.

http://www.freescale.com/webapp/Download?colCode=IMX6_KK443_200_ANDROID_DOCS&Parent_nodeId=133769948...


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
3,258 次查看
kikimorisato
Contributor II

I did not have any error messages.

I do not use proxies and firewalls.

here is my terminal screenshot

linux3.png

----------------------------------------------------------------------------------------------------------------------------------------------------------------

and here is all terminal message

kimjh@kimjh-virtual-machine:~/fsl-release-bsp-sane$ repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-3.14.28-1.0.0_ga

From git://git.freescale.com/imx/fsl-arm-yocto-bsp

* [new branch]      imx-3.10.17-1.0.0_ga -> origin/imx-3.10.17-1.0.0_ga

* [new branch]      imx-3.10.17-1.0.1_ga -> origin/imx-3.10.17-1.0.1_ga

* [new branch]      imx-3.10.17-1.0.2_ga -> origin/imx-3.10.17-1.0.2_ga

* [new branch]      imx-3.10.53-1.1.0_ga -> origin/imx-3.10.53-1.1.0_ga

* [new branch]      imx-3.10.53-1.1.1_patch -> origin/imx-3.10.53-1.1.1_patch

* [new branch]      imx-3.10.53-1.1.2_patch -> origin/imx-3.10.53-1.1.2_patch

* [new branch]      imx-3.14.28-1.0.0_ga -> origin/imx-3.14.28-1.0.0_ga

Your identity is: kimjh <****@********.***>

If you want to change this, please re-run 'repo init' with --config-name

repo has been initialized in /home/kimjh/fsl-release-bsp-sane

kimjh@kimjh-virtual-machine:~/fsl-release-bsp-sane$ repo sync

Fetching project meta-openembedded

Fetching project meta-fsl-bsp-release

From git://git.freescale.com/imx/meta-fsl-bsp-release

* [new branch]      daisy_3.10.53-1.1.0_GA -> fsl-release/daisy_3.10.53-1.1.0_GA

* [new branch]      daisy_3.10.53-1.1.1_patch -> fsl-release/daisy_3.10.53-1.1.1_patch

* [new branch]      daisy_3.10.53-1.1.2_patch -> fsl-release/daisy_3.10.53-1.1.2_patch

* [new branch]      dizzy_3.14.28-1.0.0_GA -> fsl-release/dizzy_3.14.28-1.0.0_GA

* [new branch]      dora_3.10.17-1.0.0_GA -> fsl-release/dora_3.10.17-1.0.0_GA

* [new branch]      dora_3.10.17-1.0.1 -> fsl-release/dora_3.10.17-1.0.1

* [new branch]      dora_3.10.17-1.0.2 -> fsl-release/dora_3.10.17-1.0.2

* [new branch]      master     -> fsl-release/master

* [new tag]         rel_imx_3.14.28_1.0.0_ga -> rel_imx_3.14.28_1.0.0_ga

Fetching projects:  11% (1/9)  Fetching project meta-fsl-demos

From git://github.com/Freescale/meta-fsl-demos

* [new branch]      daisy      -> freescale/daisy

* [new branch]      danny      -> freescale/danny

* [new branch]      denzil     -> freescale/denzil

* [new branch]      dizzy      -> freescale/dizzy

* [new branch]      dizzy-next -> freescale/dizzy-next

* [new branch]      dora       -> freescale/dora

* [new branch]      dylan      -> freescale/dylan

* [new branch]      fido       -> freescale/fido

* [new branch]      master     -> freescale/master

* [new branch]      master-next -> freescale/master-next

* [new tag]         1.2        -> 1.2

* [new tag]         1.2-rc1    -> 1.2-rc1

* [new tag]         1.3        -> 1.3

* [new tag]         1.4        -> 1.4

* [new tag]         1.5        -> 1.5

* [new tag]         1.6        -> 1.6

* [new tag]         1.7        -> 1.7

* [new tag]         1.8        -> 1.8

Fetching projects:  22% (2/9)  Fetching project meta-fsl-arm

From git://git.openembedded.org/meta-openembedded

* [new branch]      daisy      -> oe/daisy

* [new branch]      daisy-next -> oe/daisy-next

* [new branch]      danny      -> oe/danny

* [new branch]      danny-next -> oe/danny-next

* [new branch]      denzil     -> oe/denzil

* [new branch]      denzil-next -> oe/denzil-next

* [new branch]      dizzy      -> oe/dizzy

* [new branch]      dizzy-next -> oe/dizzy-next

* [new branch]      dora       -> oe/dora

* [new branch]      dora-next  -> oe/dora-next

* [new branch]      dylan      -> oe/dylan

* [new branch]      dylan-next -> oe/dylan-next

* [new branch]      fido       -> oe/fido

* [new branch]      fido-next  -> oe/fido-next

* [new branch]      jansa/dizzy -> oe/jansa/dizzy

* [new branch]      jansa/fido -> oe/jansa/fido

* [new branch]      jansa/master -> oe/jansa/master

* [new branch]      master     -> oe/master

* [new branch]      master-next -> oe/master-next

Fetching projects:  33% (3/9)  Fetching project meta-browser

From git://github.com/OSSystems/meta-browser

* [new branch]      danny      -> OSSystems/danny

* [new branch]      dora       -> OSSystems/dora

* [new branch]      dylan      -> OSSystems/dylan

* [new branch]      master     -> OSSystems/master

Fetching projects:  44% (4/9)  Fetching project poky

From git://git.yoctoproject.org/meta-fsl-arm

* [new branch]      1.4_M3     -> yocto/1.4_M3

* [new branch]      1.4_M5     -> yocto/1.4_M5

* [new branch]      daisy      -> yocto/daisy

* [new branch]      danny      -> yocto/danny

* [new branch]      danny-next -> yocto/danny-next

* [new branch]      denzil     -> yocto/denzil

* [new branch]      dizzy      -> yocto/dizzy

* [new branch]      dizzy-next -> yocto/dizzy-next

* [new branch]      dora       -> yocto/dora

* [new branch]      dora-next  -> yocto/dora-next

* [new branch]      dylan      -> yocto/dylan

* [new branch]      dylan-next -> yocto/dylan-next

* [new branch]      fido       -> yocto/fido

* [new branch]      master     -> yocto/master

* [new branch]      master-next -> yocto/master-next

* [new tag]         1.2        -> 1.2

* [new tag]         1.2-rc1    -> 1.2-rc1

* [new tag]         1.3        -> 1.3

* [new tag]         1.4        -> 1.4

* [new tag]         1.5        -> 1.5

* [new tag]         1.6        -> 1.6

* [new tag]         1.7        -> 1.7

* [new tag]         1.8        -> 1.8

Fetching projects:  55% (5/9)  Fetching project fsl-community-bsp-base

From git://github.com/Freescale/fsl-community-bsp-base

* [new branch]      daisy      -> freescale/daisy

* [new branch]      danny      -> freescale/danny

* [new branch]      denzil     -> freescale/denzil

* [new branch]      dizzy      -> freescale/dizzy

* [new branch]      dora       -> freescale/dora

* [new branch]      dylan      -> freescale/dylan

* [new branch]      fido       -> freescale/fido

* [new branch]      master     -> freescale/master

* [new branch]      master-next -> freescale/master-next

* [new tag]         1.2        -> 1.2

* [new tag]         1.2-rc1    -> 1.2-rc1

* [new tag]         1.3        -> 1.3

* [new tag]         1.4        -> 1.4

* [new tag]         1.5        -> 1.5

* [new tag]         1.6        -> 1.6

* [new tag]         1.7        -> 1.7

* [new tag]         1.8        -> 1.8

Fetching projects:  66% (6/9)  Fetching project meta-fsl-arm-extra

From git://github.com/Freescale/meta-fsl-arm-extra

* [new branch]      daisy      -> freescale/daisy

* [new branch]      danny      -> freescale/danny

* [new branch]      denzil     -> freescale/denzil

* [new branch]      dizzy      -> freescale/dizzy

* [new branch]      dizzy-next -> freescale/dizzy-next

* [new branch]      dora       -> freescale/dora

* [new branch]      dora-next  -> freescale/dora-next

* [new branch]      dylan      -> freescale/dylan

* [new branch]      fido       -> freescale/fido

* [new branch]      master     -> freescale/master

* [new branch]      master-next -> freescale/master-next

* [new tag]         1.2        -> 1.2

* [new tag]         1.2-rc1    -> 1.2-rc1

* [new tag]         1.3        -> 1.3

* [new tag]         1.4        -> 1.4

* [new tag]         1.5        -> 1.5

* [new tag]         1.6        -> 1.6

* [new tag]         1.7        -> 1.7

* [new tag]         1.8        -> 1.8

Fetching projects:  77% (7/9)  Fetching project meta-qt5

From git://github.com/meta-qt5/meta-qt5

* [new branch]      daisy      -> QT5/daisy

* [new branch]      dizzy      -> QT5/dizzy

* [new branch]      dora       -> QT5/dora

* [new branch]      dora-next  -> QT5/dora-next

* [new branch]      dylan      -> QT5/dylan

* [new branch]      fido       -> QT5/fido

* [new branch]      fido-next  -> QT5/fido-next

* [new branch]      jansa/daisy -> QT5/jansa/daisy

* [new branch]      jansa/dizzy -> QT5/jansa/dizzy

* [new branch]      jansa/dylan-backport -> QT5/jansa/dylan-backport

* [new branch]      jansa/fido -> QT5/jansa/fido

* [new branch]      jansa/master -> QT5/jansa/master

* [new branch]      master     -> QT5/master

* [new branch]      master-next -> QT5/master-next

* [new branch]      otavio/master -> QT5/otavio/master

* [new tag]         5.2.1+origin/release -> 5.2.1+origin/release

* [new tag]         jansa/test-2013-10-08 -> jansa/test-2013-10-08

* [new tag]         master-next-2014-02-19 -> master-next-2014-02-19

Fetching projects:  88% (8/9)  From git://git.yoctoproject.org/poky

* [new branch]      1.1_M1     -> yocto/1.1_M1

* [new branch]      1.1_M2     -> yocto/1.1_M2

* [new branch]      1.1_M3     -> yocto/1.1_M3

* [new branch]      1.1_M4     -> yocto/1.1_M4

* [new branch]      1.2_M1     -> yocto/1.2_M1

* [new branch]      1.2_M2     -> yocto/1.2_M2

* [new branch]      1.2_M3     -> yocto/1.2_M3

* [new branch]      1.2_M4     -> yocto/1.2_M4

* [new branch]      1.3_M1     -> yocto/1.3_M1

* [new branch]      1.3_M2     -> yocto/1.3_M2

* [new branch]      1.3_M3     -> yocto/1.3_M3

* [new branch]      1.3_M4     -> yocto/1.3_M4

* [new branch]      1.3_M5     -> yocto/1.3_M5

* [new branch]      1.3_beta   -> yocto/1.3_beta

* [new branch]      1.4_M1     -> yocto/1.4_M1

* [new branch]      1.4_M3     -> yocto/1.4_M3

* [new branch]      1.4_M4     -> yocto/1.4_M4

* [new branch]      1.4_M5     -> yocto/1.4_M5

* [new branch]      1.6_M5     -> yocto/1.6_M5

* [new branch]      bernard    -> yocto/bernard

* [new branch]      blinky     -> yocto/blinky

* [new branch]      clyde      -> yocto/clyde

* [new branch]      daisy      -> yocto/daisy

* [new branch]      danny      -> yocto/danny

* [new branch]      danny-next -> yocto/danny-next

* [new branch]      denzil     -> yocto/denzil

* [new branch]      dizzy      -> yocto/dizzy

* [new branch]      dora       -> yocto/dora

* [new branch]      dora-toaster -> yocto/dora-toaster

* [new branch]      dylan      -> yocto/dylan

* [new branch]      edison     -> yocto/edison

* [new branch]      elroy      -> yocto/elroy

* [new branch]      fido       -> yocto/fido

* [new branch]      green      -> yocto/green

* [new branch]      laverne    -> yocto/laverne

* [new branch]      master     -> yocto/master

* [new branch]      master-next -> yocto/master-next

* [new branch]      pinky      -> yocto/pinky

* [new branch]      purple     -> yocto/purple

* [new tag]         1.1_M1.final -> 1.1_M1.final

* [new tag]         1.1_M1.rc1 -> 1.1_M1.rc1

* [new tag]         1.1_M1.rc2 -> 1.1_M1.rc2

* [new tag]         1.1_M2.final -> 1.1_M2.final

* [new tag]         1.1_M2.rc1 -> 1.1_M2.rc1

* [new tag]         1.1_M2.rc2 -> 1.1_M2.rc2

* [new tag]         1.1_M2.rc3 -> 1.1_M2.rc3

* [new tag]         1.1_M3.final -> 1.1_M3.final

* [new tag]         1.1_M3.rc2 -> 1.1_M3.rc2

* [new tag]         1.1_M3.rc3 -> 1.1_M3.rc3

* [new tag]         1.1_M4.rc2+ -> 1.1_M4.rc2+

* [new tag]         1.1_M4.rc3 -> 1.1_M4.rc3

* [new tag]         1.1_M4.rc4 -> 1.1_M4.rc4

* [new tag]         1.2_M1.final -> 1.2_M1.final

* [new tag]         1.2_M1.rc1 -> 1.2_M1.rc1

* [new tag]         1.2_M1.rc2 -> 1.2_M1.rc2

* [new tag]         1.2_M2.final -> 1.2_M2.final

* [new tag]         1.2_M2.rc1 -> 1.2_M2.rc1

* [new tag]         1.2_M3.final -> 1.2_M3.final

* [new tag]         1.2_M3.rc1 -> 1.2_M3.rc1

* [new tag]         1.2_M4.rc1 -> 1.2_M4.rc1

* [new tag]         1.2_M4.rc2 -> 1.2_M4.rc2

* [new tag]         1.2_M4.rc3 -> 1.2_M4.rc3

* [new tag]         1.2_M4.rc3.1 -> 1.2_M4.rc3.1

* [new tag]         1.2_M4.rc3.2 -> 1.2_M4.rc3.2

* [new tag]         1.2_M4.rc4 -> 1.2_M4.rc4

* [new tag]         1.2_M4.rc4.0 -> 1.2_M4.rc4.0

* [new tag]         1.3        -> 1.3

* [new tag]         1.3.1      -> 1.3.1

* [new tag]         1.3.2      -> 1.3.2

* [new tag]         1.3.2.final -> 1.3.2.final

* [new tag]         1.3_M1.final -> 1.3_M1.final

* [new tag]         1.3_M1.rc1 -> 1.3_M1.rc1

* [new tag]         1.3_M2.final -> 1.3_M2.final

* [new tag]         1.3_M2.rc1 -> 1.3_M2.rc1

* [new tag]         1.3_M3.final -> 1.3_M3.final

* [new tag]         1.3_M3.rc2 -> 1.3_M3.rc2

* [new tag]         1.3_M4.final -> 1.3_M4.final

* [new tag]         1.3_M4.rc1 -> 1.3_M4.rc1

* [new tag]         1.3_M5.rc1 -> 1.3_M5.rc1

* [new tag]         1.3_M5.rc2 -> 1.3_M5.rc2

* [new tag]         1.3_M5.rc3 -> 1.3_M5.rc3

* [new tag]         1.3_M5.rc4 -> 1.3_M5.rc4

* [new tag]         1.4.1.rc1  -> 1.4.1.rc1

* [new tag]         1.4_M1.final -> 1.4_M1.final

* [new tag]         1.4_M1.rc1 -> 1.4_M1.rc1

* [new tag]         1.4_M3.final -> 1.4_M3.final

* [new tag]         1.4_M3.rc1 -> 1.4_M3.rc1

* [new tag]         1.4_M3.rc2 -> 1.4_M3.rc2

* [new tag]         1.4_M4.final -> 1.4_M4.final

* [new tag]         1.4_M4.rc1 -> 1.4_M4.rc1

* [new tag]         1.4_M5.final -> 1.4_M5.final

* [new tag]         1.4_M5.rc1 -> 1.4_M5.rc1

* [new tag]         1.4_M5.rc2 -> 1.4_M5.rc2

* [new tag]         1.4_M5.rc3 -> 1.4_M5.rc3

* [new tag]         1.4_M6.rc1 -> 1.4_M6.rc1

* [new tag]         1.5_M1.final -> 1.5_M1.final

* [new tag]         1.5_M1.rc1 -> 1.5_M1.rc1

* [new tag]         1.5_M2.rc1 -> 1.5_M2.rc1

* [new tag]         1.5_M3     -> 1.5_M3

* [new tag]         1.5_M3.final -> 1.5_M3.final

* [new tag]         1.5_M3.rc1 -> 1.5_M3.rc1

* [new tag]         1.5_M4     -> 1.5_M4

* [new tag]         1.5_M4.final -> 1.5_M4.final

* [new tag]         1.5_M4.rc1 -> 1.5_M4.rc1

* [new tag]         1.5_M4.rc2 -> 1.5_M4.rc2

* [new tag]         1.5_M4.rc3 -> 1.5_M4.rc3

* [new tag]         1.5_M5.rc1 -> 1.5_M5.rc1

* [new tag]         1.5_M5.rc2 -> 1.5_M5.rc2

* [new tag]         1.5_M5.rc3 -> 1.5_M5.rc3

* [new tag]         1.5_M5.rc4 -> 1.5_M5.rc4

* [new tag]         1.5_M5.rc5 -> 1.5_M5.rc5

* [new tag]         1.5_M5.rc6 -> 1.5_M5.rc6

* [new tag]         1.5_M5.rc7 -> 1.5_M5.rc7

* [new tag]         1.5_M5.rc8 -> 1.5_M5.rc8

* [new tag]         1.6_M1     -> 1.6_M1

* [new tag]         1.6_M1.final -> 1.6_M1.final

* [new tag]         1.6_M1.rc1 -> 1.6_M1.rc1

* [new tag]         1.6_M2     -> 1.6_M2

* [new tag]         1.6_M3     -> 1.6_M3

* [new tag]         1.6_M3.final -> 1.6_M3.final

* [new tag]         1.6_M4     -> 1.6_M4

* [new tag]         1.7_M1     -> 1.7_M1

* [new tag]         1.7_M2     -> 1.7_M2

* [new tag]         1.7_M3     -> 1.7_M3

* [new tag]         1.8_M1     -> 1.8_M1

* [new tag]         1.8_M2     -> 1.8_M2

* [new tag]         1.8_M3     -> 1.8_M3

* [new tag]         bernard-1.0rc1 -> bernard-1.0rc1

* [new tag]         bernard-5.0 -> bernard-5.0

* [new tag]         bernard-5.0-alpha -> bernard-5.0-alpha

* [new tag]         bernard-5.0.1 -> bernard-5.0.1

* [new tag]         bernard-5.0.2 -> bernard-5.0.2

* [new tag]         bernard-5.0.2+docs -> bernard-5.0.2+docs

* [new tag]         bernard-5.0rc1 -> bernard-5.0rc1

* [new tag]         bernard-5.0rc2 -> bernard-5.0rc2

* [new tag]         blinky-3.0 -> blinky-3.0

* [new tag]         clyde-2.0  -> clyde-2.0

* [new tag]         daisy-11.0.0 -> daisy-11.0.0

* [new tag]         daisy-11.0.1 -> daisy-11.0.1

* [new tag]         daisy-11.0.2 -> daisy-11.0.2

* [new tag]         danny-8.0  -> danny-8.0

* [new tag]         danny-8.0.1 -> danny-8.0.1

* [new tag]         danny-8.0.2 -> danny-8.0.2

* [new tag]         denzil-7.0 -> denzil-7.0

* [new tag]         denzil-7.0.0 -> denzil-7.0.0

* [new tag]         denzil-7.0.1 -> denzil-7.0.1

* [new tag]         denzil-7.0.1_rc2 -> denzil-7.0.1_rc2

* [new tag]         denzil-7.0.2 -> denzil-7.0.2

* [new tag]         dizzy-12.0.0 -> dizzy-12.0.0

* [new tag]         dizzy-12.0.1 -> dizzy-12.0.1

* [new tag]         dora-10.0.0 -> dora-10.0.0

* [new tag]         dora-10.0.0.final -> dora-10.0.0.final

* [new tag]         dora-10.0.1 -> dora-10.0.1

* [new tag]         dora-10.0.1.final -> dora-10.0.1.final

* [new tag]         dora-10.0.2 -> dora-10.0.2

* [new tag]         dora-10.0.3 -> dora-10.0.3

* [new tag]         dora-10.0.4 -> dora-10.0.4

* [new tag]         dylan-9.0.0 -> dylan-9.0.0

* [new tag]         dylan-9.0.1 -> dylan-9.0.1

* [new tag]         dylan-9.0.1.rc1 -> dylan-9.0.1.rc1

* [new tag]         dylan-9.0.2 -> dylan-9.0.2

* [new tag]         dylan-9.0.2.rc1 -> dylan-9.0.2.rc1

* [new tag]         dylan-9.0.3 -> dylan-9.0.3

* [new tag]         dylan-9.0.4 -> dylan-9.0.4

* [new tag]         edison-6.0 -> edison-6.0

* [new tag]         edison-6.0.1 -> edison-6.0.1

* [new tag]         edison-6.0.1.final -> edison-6.0.1.final

* [new tag]         edison-6.0.1.release -> edison-6.0.1.release

* [new tag]         edison-6.0.2 -> edison-6.0.2

* [new tag]         edison-6.0.2_rc1 -> edison-6.0.2_rc1

* [new tag]         fido-13.0.0 -> fido-13.0.0

* [new tag]         green-3.3  -> green-3.3

* [new tag]         green-3.3.1 -> green-3.3.1

* [new tag]         inky-1.0   -> inky-1.0

* [new tag]         laverne-4.0 -> laverne-4.0

* [new tag]         laverne-4.0.1 -> laverne-4.0.1

* [new tag]         pinky-3.1  -> pinky-3.1

* [new tag]         pinky-3.1.1 -> pinky-3.1.1

* [new tag]         pinky-3.1.2 -> pinky-3.1.2

* [new tag]         poky-10.0.0.final -> poky-10.0.0.final

* [new tag]         purple-3.2 -> purple-3.2

* [new tag]         purple-3.2.1 -> purple-3.2.1

* [new tag]         toaster-dora-10.0.0 -> toaster-dora-10.0.0

* [new tag]         yocot-1.4.2 -> yocot-1.4.2

* [new tag]         yocto-1.4.1 -> yocto-1.4.1

* [new tag]         yocto-1.4.2 -> yocto-1.4.2

* [new tag]         yocto-1.4.2.rc1 -> yocto-1.4.2.rc1

* [new tag]         yocto-1.4.3 -> yocto-1.4.3

* [new tag]         yocto-1.4.4 -> yocto-1.4.4

* [new tag]         yocto-1.5  -> yocto-1.5

* [new tag]         yocto-1.5.1 -> yocto-1.5.1

* [new tag]         yocto-1.5.1.final -> yocto-1.5.1.final

* [new tag]         yocto-1.5.2 -> yocto-1.5.2

* [new tag]         yocto-1.5.3 -> yocto-1.5.3

* [new tag]         yocto-1.5.4 -> yocto-1.5.4

* [new tag]         yocto-1.5.final -> yocto-1.5.final

* [new tag]         yocto-1.5_M5.rc2 -> yocto-1.5_M5.rc2

* [new tag]         yocto-1.6  -> yocto-1.6

* [new tag]         yocto-1.6.1 -> yocto-1.6.1

* [new tag]         yocto-1.6.2 -> yocto-1.6.2

* [new tag]         yocto-1.7  -> yocto-1.7

* [new tag]         yocto-1.7.1 -> yocto-1.7.1

* [new tag]         yocto-1.8  -> yocto-1.8

* [new tag]         yocto_1.5_M5.rc8 -> yocto_1.5_M5.rc8

Fetching projects: 100% (9/9), done.

kimjh@kimjh-virtual-machine:~/fsl-release-bsp-sane$

0 项奖励
回复
3,258 次查看
Yuri
NXP Employee
NXP Employee

  So, all looks OK. What is the problem ?

Can You continue system building as recommended in "Freescale_Yocto_Project_User's_Guide.pdf" ?

Note, the directory fsl-release-bsp[-sane]/sources really contains only instructions how
to load OS sources and build the images.

Regards,

Yuri.

0 项奖励
回复
3,258 次查看
kikimorisato
Contributor II

the problem is imx-linux version is 3.0.17 (and all recipes from "imx-3.10.17-1.0.0_ga")

when i used fsl-community-bsp

recipes-kernel version is linux-imx-3.14.28

and bb file included 3.14.28

but fsl-release-bsp(imx-3.14.28-1.0.0_ga branch)'s recipes-kernel version is linux-imx-3.10.17

also bb file included 3.10.17

bitbake -c compile -f linux-imx ==> than linux-imx compiled 3.10.17

----------------------------------------------------------------------------------------------------------------------------------------

i want use imx-3.14.28-1.0.0_ga branch and linux-imx 3.14.28

when i used fsl-community-bsp than everything is OK

but fsl-release-bsp is only 3.10.17

for examples

repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b origin/imx-3.10.53-1.1.1_patch

or

repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b origin/imx-3.10.53-1.1.2_patch


than recipes-kernel version is linux-imx-3.10.17


----------------------------------------------------------------------------------------------------------------------------------------


imx-linux-3.10.17 from linux kernel 3.14 (linux-3.14.tar.xz)

imx-linux-3.14.28 form linux kernel 3.19 (linux-3.19.tar.xz)

0 项奖励
回复
3,259 次查看
Yuri
NXP Employee
NXP Employee

Freescale BSP Release options are located in "meta-fsl-bsp-release" directory.

Regards,

Yuri

0 项奖励
回复
3,258 次查看
kikimorisato
Contributor II

thank you Yuri~~

0 项奖励
回复