Hi, NXP (freescale) support expert,
I try to light my lvds panel by a wandboard solo board, I edit the dts and get the error " ldb ldb.13: crtc not specified or invalid",
I think the reason is i place the script: crtcs = <0xf 0x0>; i think it is not correct ,so pls tell me how to write it, looking forward to reply, thanks.
my dts is the following, :
| fb@0 { | |
| compatible = "fsl,mxc_sdc_fb"; | |
| disp_dev = "ldb"; | |
| interface_pix_fmt = "RGB24"; | |
| mode_str = "LP101WH4-SLAA"; | |
| default_bpp = <0x20>; | |
| int_clk = <0x0>; | |
| late_init = <0x0>; | |
| status = "okay"; | 
};
| ldb@020e0008 { | |||
| #address-cells = <0x1>; | |||
| #size-cells = <0x0>; | |||
| gpr = <0xa>; | |||
| status = "okay"; | |||
| compatible = "fsl,imx6dl-ldb", "fsl,imx53-ldb"; | |||
| clocks = <0x2 0x87 0x2 0x88 0x2 0x27 0x2 0x28 0x2 0x29 0x2 0xb8 0x2 0xb9 0x2 0xd1 0x2 0xd2 0x2 0xd3 0x2 0xd4>; | |||
| clock-names = "ldb_di0", "ldb_di1", "di0_sel", "di1_sel", "di2_sel", "ldb_di0_div_3_5", "ldb_di1_div_3_5", "ldb_di0_div_7", "ldb_di1_div_7", "ldb_di0_div_sel", "ldb_di1_div_sel"; | 
| lvds-channel@0 { | ||||
| reg = <0x0>; | ||||
| status = "okay"; | ||||
| crtcs = <0xf 0x0>; | ||||
| fsl,data-mapping = "spwg"; | ||||
| fsl,data-width = <0x18>; | 
| display-timings { | |||||
| native-mode = <0x10>; | 
| LP101WH4-SLAA { | ||||||
| clock-frequency = <0x44aa200>; | ||||||
| hactive = <0x556>; | ||||||
| vactive = <0x300>; | ||||||
| hfront-porch = <0x50>; | ||||||
| hback-porch = <0x30>; | ||||||
| hsync-len = <0x20>; | ||||||
| vback-porch = <0xe>; | ||||||
| vfront-porch = <0x3>; | ||||||
| vsync-len = <0x5>; | ||||||
| hsync-active = <0x0>; | ||||||
| vsync-active = <0x0>; | ||||||
| linux,phandle = <0x10>; | ||||||
| phandle = <0x10>; | ||||||
| }; | ||||||
| }; | ||||||
| }; | 
| lvds-channel@1 { | ||||
| reg = <0x1>; | ||||
| status = "disabled"; | ||||
| }; | 
Hi wz
one can look at "crtcs" linux documentation and example:
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------