imx6sololite usb otg As Wakeup source cannot wakeup screen,only wakeup system

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6sololite usb otg As Wakeup source cannot wakeup screen,only wakeup system

953件の閲覧回数
kangzhikuan
Contributor II

imx6sololite usb otg As Wakeup source cannot wakeup screen,only wakeup system。I hope you can help me

0 件の賞賛
返信
1 返信

774件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi,

Below you can find some threads and an application note regarding USB configuration on i.MX6:

Power State Wakeup accepted interrupts and wakeup times for IMX6 SoloLite?

iMX6 SABRE SD can't see USB mouse and keyboard

http://www.nxp.com/files/32bit/doc/app_note/AN4589.pdf


Hope this will be useful for you.
Best regards!
/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信