help uboot porting SD4

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

help uboot porting SD4

3,996件の閲覧回数
lixuhui112
Contributor I

In my board only have sd4 look at pg1

sd .png

                                                            pg1

the code such as :

configs file :

#define CONFIG_FSL_ESDHC

#define CONFIG_FSL_USDHC

#define CONFIG_SYS_FSL_ESDHC_ADDR      USDHC4_BASE_ADDR

#define CONFIG_MMCROOT   "/dev/mmcblk3p2"  /* SDHC4 */

#define CONFIG_SYS_FSL_USDHC_NUM    3

#define CONFIG_SYS_MMC_ENV_DEV   2  /* SDHC4 */
#define CONFIG_SYS_MMC_ENV_PART            0   /* user partition */

borad .c

tatic iomux_v3_cfg_t const usdhc4_pads[] = {

    MX6_PAD_SD4_CLK__SD4_CLK   | MUX_PAD_CTRL(USDHC_PAD_CTRL),

    MX6_PAD_SD4_CMD__SD4_CMD   | MUX_PAD_CTRL(USDHC_PAD_CTRL),

    MX6_PAD_SD4_DAT0__SD4_DATA0 | MUX_PAD_CTRL(USDHC_PAD_CTRL),

    MX6_PAD_SD4_DAT1__SD4_DATA1 | MUX_PAD_CTRL(USDHC_PAD_CTRL),

    MX6_PAD_SD4_DAT2__SD4_DATA2 | MUX_PAD_CTRL(USDHC_PAD_CTRL),

    MX6_PAD_SD4_DAT3__SD4_DATA3 | MUX_PAD_CTRL(USDHC_PAD_CTRL),

    MX6_PAD_SD4_DAT4__SD4_DATA4 | MUX_PAD_CTRL(USDHC_PAD_CTRL),

    MX6_PAD_SD4_DAT5__SD4_DATA5 | MUX_PAD_CTRL(USDHC_PAD_CTRL),

    MX6_PAD_SD4_DAT6__SD4_DATA6 | MUX_PAD_CTRL(USDHC_PAD_CTRL),

    MX6_PAD_SD4_DAT7__SD4_DATA7 | MUX_PAD_CTRL(USDHC_PAD_CTRL),

        /* CD */

        MX6_PAD_SD1_DAT0__GPIO1_IO16    | MUX_PAD_CTRL(NO_PAD_CTRL),

};

#ifdef CONFIG_FSL_ESDHC

struct fsl_esdhc_cfg usdhc_cfg[1] = {

//    {USDHC2_BASE_ADDR},

//    {USDHC3_BASE_ADDR},

    {USDHC4_BASE_ADDR},

};

int mmc_get_env_devno(void)

{

    u32 soc_sbmr = readl(SRC_BASE_ADDR + 0x4);

    u32 dev_no;

    u32 bootsel;

    bootsel = (soc_sbmr & 0x000000FF) >> 6 ;

    /* If not boot from sd/mmc, use default value */

    if (bootsel != 1)

        return CONFIG_SYS_MMC_ENV_DEV;

    /* BOOT_CFG2[3] and BOOT_CFG2[4] */

    dev_no = (soc_sbmr & 0x00001800) >> 11;

    /* need ubstract 1 to map to the mmc device id

     * see the comments in board_mmc_init function

     */

    dev_no--;

    return dev_no;

}

int mmc_map_to_kernel_blk(int dev_no)

{

    return dev_no + 1;

}

//#define USDHC2_CD_GPIO    IMX_GPIO_NR(2, 2)

#define USDHC4_CD_GPIO    IMX_GPIO_NR(1, 16)

int board_mmc_getcd(struct mmc *mmc)

{

    struct fsl_esdhc_cfg *cfg = (struct fsl_esdhc_cfg *)mmc->priv;

    int ret = 0;

    switch (cfg->esdhc_base) {

//    case USDHC2_BASE_ADDR:

    //    ret = !gpio_get_value(USDHC2_CD_GPIO);

        //break;

    //case USDHC3_BASE_ADDR:

        //ret = !gpio_get_value(USDHC3_CD_GPIO);

    //    break;

    case USDHC4_BASE_ADDR:

                ret = !gpio_get_value(USDHC4_CD_GPIO);

       //         ret = 1; /* eMMC/uSDHC4 is always present */

        break;

    }

    return ret;

}

int board_mmc_init(bd_t *bis)

{

#ifndef CONFIG_SPL_BUILD

    int ret;

    int i;

    /*

     * According to the board_mmc_init() the following map is done:

     * (U-boot device node)    (Physical Port)

     * mmc0                    SD2

     * mmc1                    SD3

     * mmc2                    SD4

     */

    for (i = 0; i < CONFIG_SYS_FSL_USDHC_NUM; i++) {

        switch :smileyinfo: {

    //    case 0:

    //        imx_iomux_v3_setup_multiple_pads(

    //            usdhc2_pads, ARRAY_SIZE(usdhc2_pads));

    //        gpio_direction_input(USDHC2_CD_GPIO);

    //        usdhc_cfg[0].sdhc_clk = mxc_get_clock(MXC_ESDHC2_CLK);

    //        break;

    //    case 1:

    //        imx_iomux_v3_setup_multiple_pads(

    //            usdhc3_pads, ARRAY_SIZE(usdhc3_pads));

    //        gpio_direction_input(USDHC3_CD_GPIO);

    //        usdhc_cfg[1].sdhc_clk = mxc_get_clock(MXC_ESDHC3_CLK);

    //        break;

        case 2:

            imx_iomux_v3_setup_multiple_pads(

                usdhc4_pads, ARRAY_SIZE(usdhc4_pads));

                        gpio_direction_input(USDHC4_CD_GPIO);

            usdhc_cfg[2].sdhc_clk = mxc_get_clock(MXC_ESDHC4_CLK);

            break;

        default:

            printf("Warning: you configured more USDHC controllers"

                   "(%d) then supported by the board (%d)\n",

                   i + 1, CONFIG_SYS_FSL_USDHC_NUM);

            return -EINVAL;

        }

        ret = fsl_esdhc_initialize(bis, &usdhc_cfg[i]);

        if (ret)

            return ret;

    }

    return 0;

#else

    struct src *psrc = (struct src *)SRC_BASE_ADDR;

    unsigned reg = readl(&psrc->sbmr1) >> 11;

    /*

     * Upon reading BOOT_CFG register the following map is done:

     * Bit 11 and 12 of BOOT_CFG register can determine the current

     * mmc port

     * 0x1                  SD1

     * 0x2                  SD2

     * 0x3                  SD4

     */

    switch (reg & 0x3) {

//    case 0x1:

//        imx_iomux_v3_setup_multiple_pads(

//            usdhc2_pads, ARRAY_SIZE(usdhc2_pads));

//        usdhc_cfg[0].esdhc_base = USDHC2_BASE_ADDR;

//        usdhc_cfg[0].sdhc_clk = mxc_get_clock(MXC_ESDHC2_CLK);

//        gd->arch.sdhc_clk = usdhc_cfg[0].sdhc_clk;

//        break;

//    case 0x2:

//        imx_iomux_v3_setup_multiple_pads(

//            usdhc3_pads, ARRAY_SIZE(usdhc3_pads));

//        usdhc_cfg[0].esdhc_base = USDHC3_BASE_ADDR;

//        usdhc_cfg[0].sdhc_clk = mxc_get_clock(MXC_ESDHC3_CLK);

//        gd->arch.sdhc_clk = usdhc_cfg[0].sdhc_clk;

//        break;

    case 0x3:

        imx_iomux_v3_setup_multiple_pads(

            usdhc4_pads, ARRAY_SIZE(usdhc4_pads));

        usdhc_cfg[0].esdhc_base = USDHC4_BASE_ADDR;

        usdhc_cfg[0].sdhc_clk = mxc_get_clock(MXC_ESDHC4_CLK);

        gd->arch.sdhc_clk = usdhc_cfg[0].sdhc_clk;

        break;

    }

    return fsl_esdhc_initialize(bis, &usdhc_cfg[0]);

#endif

}

#endif

int check_mmc_autodetect(void)

{

    char *autodetect_str = getenv("mmcautodetect");

    if ((autodetect_str != NULL) &&

        (strcmp(autodetect_str, "yes") == 0)) {

        return 1;

    }

    return 0;

}

void board_late_mmc_env_init(void)

{

    char cmd[32];

    char mmcblk[32];

    u32 dev_no = mmc_get_env_devno();

    if (!check_mmc_autodetect())

        return;

    setenv_ulong("mmcdev", dev_no);

    /* Set mmcblk env */

    sprintf(mmcblk, "/dev/mmcblk%dp2 rootwait rw",

        mmc_map_to_kernel_blk(dev_no));

    setenv("mmcroot", mmcblk);

    sprintf(cmd, "mmc dev %d", dev_no);

    run_command(cmd, 0);

}

#ifdef CONFIG_CMD_BMODE

static const struct boot_mode board_boot_modes[] = {

    /* 4 bit bus width */

    {"sd4", MAKE_CFGVAL(0x40, 0x38, 0x00, 0x00)},

    {NULL,   0},

};

#endif

int board_late_init(void)

{

#ifdef CONFIG_CMD_BMODE

    add_board_boot_modes(board_boot_modes);

#endif

#ifdef CONFIG_ENV_IS_IN_MMC

    board_late_mmc_env_init();

#endif

    return 0;

}

build  u-boot.imx   ,but  i can not find sd4,as :

U-Boot 2015.04-14468-gd7d7c43-dirty (Jun 22 2016 - 15:02:33)

CPU:   Freescale i.MX6Q rev1.5 at 792 MHz

CPU:   Temperature 38 C

Reset cause: POR

Board: MX6Q-Sabreauto revA

I2C:   ready

DRAM:  1 GiB

PMIC:  PFUZE100 ID=0x10

MMC:   Warning: you configured more USDHC controllers(1) then supported by the board (3)

FSL_SDHC: 0

MMC Device 2 not found

No MMC card found

Using default environment

In:    serial

Out:   serial

Err:   serial

MMC Device 2 not found

no mmc device at slot 2

Net:   FEC [PRIME]

Error: FEC address not set.

Boot from USB for mfgtools

Use default environment for                              mfgtools

Run bootcmd_mfg: run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr};

Hit any key to stop autoboot:  0

Bad Linux ARM zImage magic!

=>

Thanks

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

2,976件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi xuhui

please refer to attached Porting Guide

Chapter 4 Adding Support for SDHC

Also SD4 is supported for SabreSD board (emmc) and

one can look at uboot sources in

uboot-imx.git - Freescale i.MX u-boot Tree

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,976件の閲覧回数
lixuhui112
Contributor I

yes I look the Porting Guide and you can look my code ,it is Modified in accordance with mx6sabresd.c ,but it is not ok

0 件の賞賛
返信