hardware acceleration supporting of directfb in directfb v1.6 in yocto "dylan"

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

hardware acceleration supporting of directfb in directfb v1.6 in yocto "dylan"

跳至解决方案
2,310 次查看
jojorong
Contributor IV

Hi,

     because of the hardware acceleration of directfb with version 1.4.0 is not match with in dylan (v1.6.1),

     

     so, there is someone is supporting(developing) this to make it's valid also in dylan ?

标签 (3)
1 解答
1,505 次查看
daiane_angolini
NXP Employee
NXP Employee

I think you were already replied in meta-freescale :smileywink:

Just in case other people are looking for this:

https://lists.yoctoproject.org/pipermail/meta-freescale/2013-May/002685.html

在原帖中查看解决方案

3 回复数
1,506 次查看
daiane_angolini
NXP Employee
NXP Employee

I think you were already replied in meta-freescale :smileywink:

Just in case other people are looking for this:

https://lists.yoctoproject.org/pipermail/meta-freescale/2013-May/002685.html

1,505 次查看
jojorong
Contributor IV

Hi,

But …. unfortunate, maybe there is a bug about for HW acceleration of DirectFB v1.4.0 about for "can not display cursor when moving to HW accelerated DirectFB "

It's normal to display cursor when i disable HW acceleration of DirecFB,

in the HW acceleration case, when i move the cursor to the DFB surface,

it disappear (it looks like the surface is top on the cursor).

It''s a bug ? Maybe cursor need to be HW accelerated also ?

I use the GTK+(v2.24.15) top on DirectFB(v1.4.0).

Thanks,

- Jojo

在 2013年5月16日星期四,上午2:17,Daiane Angolini 写道:

hardware acceleration supporting of directfb in directfb v1.6 in yocto "dylan"

created by Daiane Angolini (https://community.freescale.com/people/DaianeAngolini) in i.MX Community - View the full discussion (https://community.freescale.com/message/329526#329526)

I think you were already replied in meta-freescale :smileywink:

Reply to this message by replying to this email -or- go to the message on Freescale Community (https://community.freescale.com/message/329526#329526)

Start a new discussion in i.MX Community by email (mailto:discussions-community-imx@freescale-phx.hosted.jivesoftware.com ) or at Freescale Community (https://community.freescale.com/choose-container.jspa?contentType=1&containerType=14&container=2004)

>

0 项奖励
回复
1,505 次查看
daiane_angolini
NXP Employee
NXP Employee

I´m sorry, I don´t know what´s the expected behavior for DirectFB.

I hope someone else in community knows

0 项奖励
回复