hardware acceleration supporting of directfb in directfb v1.6 in yocto "dylan"

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

hardware acceleration supporting of directfb in directfb v1.6 in yocto "dylan"

ソリューションへジャンプ
2,313件の閲覧回数
jojorong
Contributor IV

Hi,

     because of the hardware acceleration of directfb with version 1.4.0 is not match with in dylan (v1.6.1),

     

     so, there is someone is supporting(developing) this to make it's valid also in dylan ?

ラベル(3)
1 解決策
1,508件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee

I think you were already replied in meta-freescale :smileywink:

Just in case other people are looking for this:

https://lists.yoctoproject.org/pipermail/meta-freescale/2013-May/002685.html

元の投稿で解決策を見る

3 返答(返信)
1,509件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee

I think you were already replied in meta-freescale :smileywink:

Just in case other people are looking for this:

https://lists.yoctoproject.org/pipermail/meta-freescale/2013-May/002685.html

1,508件の閲覧回数
jojorong
Contributor IV

Hi,

But …. unfortunate, maybe there is a bug about for HW acceleration of DirectFB v1.4.0 about for "can not display cursor when moving to HW accelerated DirectFB "

It's normal to display cursor when i disable HW acceleration of DirecFB,

in the HW acceleration case, when i move the cursor to the DFB surface,

it disappear (it looks like the surface is top on the cursor).

It''s a bug ? Maybe cursor need to be HW accelerated also ?

I use the GTK+(v2.24.15) top on DirectFB(v1.4.0).

Thanks,

- Jojo

在 2013年5月16日星期四,上午2:17,Daiane Angolini 写道:

hardware acceleration supporting of directfb in directfb v1.6 in yocto "dylan"

created by Daiane Angolini (https://community.freescale.com/people/DaianeAngolini) in i.MX Community - View the full discussion (https://community.freescale.com/message/329526#329526)

I think you were already replied in meta-freescale :smileywink:

Reply to this message by replying to this email -or- go to the message on Freescale Community (https://community.freescale.com/message/329526#329526)

Start a new discussion in i.MX Community by email (mailto:discussions-community-imx@freescale-phx.hosted.jivesoftware.com ) or at Freescale Community (https://community.freescale.com/choose-container.jspa?contentType=1&containerType=14&container=2004)

>

0 件の賞賛
返信
1,508件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee

I´m sorry, I don´t know what´s the expected behavior for DirectFB.

I hope someone else in community knows

0 件の賞賛
返信