gst1-imx plugin not working to decode the Audio AAC file

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

gst1-imx plugin not working to decode the Audio AAC file

756件の閲覧回数
adityanagal
Contributor III

Hi ,

 

I am trying to decode the AAC audio file using the following pipeline. But it is giving the error. Could somebody please suggest me the correct pipeline to decode the AAC file. imxuniaudiodec is the element of the plugin gst1-imx.

 

gst-launch-1.0 filesrc location=/mnt/Audio_Files/sample.aac ! imxuniaudiodec ! alsasink device="hw:0,0"

 

Error output :

 

Setting pipeline to PAUSED ...
Pipeline is PREROLLING ...
ERROR: from element /GstPipeline:pipeline0/GstFileSrc:filesrc0: Internal data flow error.
Additional debug info:
gstbasesrc.c(2948): gst_base_src_loop (): /GstPipeline:pipeline0/GstFileSrc:filesrc0:
streaming task paused, reason error (-5)
ERROR: pipeline doesn't want to preroll.
Setting pipeline to NULL ...
Freeing pipeline ...

 

What will be the correct pipeline ? 

Thanks,

Aditya Nagal

ラベル(2)
0 件の賞賛
返信
0 返答(返信)