i.MX6solo Gated Mode phase question.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6solo Gated Mode phase question.

768 Views
takashitakahash
Contributor III
37.4.3.6.1 Gated Mode.pngDear community.
Our customer has question below.
In the following figure of 37.4.3.6.1  of i.MX6SDL Reference manual, data reading is done at the falling edge of clock,
Can it be read at the rising edge of clock?
Is there a function to invert the clock latch phase?
Fig1.png
Data sheet of IMX6SDLAEC described on page 94, it is rising edge, which is collect?
Fig2.png
Labels (1)
0 Kudos
Reply
1 Reply

675 Views
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

you are right it is rising edge and clock polarity can be changed using CSI0_SENS_PIX_CLK_POL

bit register IPU_CSI0_SENS_CONF, described in 38.5.151 CSI0 Sensor Configuration

Register (IPU_CSI0_SENS_CONF) i.MX6SDL Reference Manual

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SDLRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply