Hi,
My issus is gpio key can not wake up system sometimes !
Linux version 3.0.35 + imx6dq + two gpio keys.
Two gpio keys:key1,key2 with wakeup feature.
App read key1 input pressed event and then "stanby" system, press key2 wakeup system. but sometimes ,key2 can not wakeup system.
As can not wake up system by press key2, I wake up system by press key1. gpio key driver produce key1 and key2 interrupt. and I check gpc IRQ masking regs: mask bits is right.
Thanks!
Hi echo
one can narrow down issue running test with baremetal sdk found on
https://community.nxp.com/thread/432859
or with minimal linux image
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igor
Sorry for your answer, I can not understand what relation between gpio wake up interrupt and SMP enable in IMX6.
I already checked the gpc mask bits setting is right.
It is difficult to debug after system suspended, so can you give me some suggestions to find out why gpio can not wake up system? My meaning is I need more details.
Best regards
echo zeng
Hi echo
this may be caused by many reasons, including ERR007265,ERR006223
errata, operating system delays/race conditions and probably old this 3.0.35 kernel version bugs.
You can follow either debug path to narrow down issue.
Best regards
igor
3.0.35 kernel is very old, since then many gpu and arm errata were fixed in new
linux bsps (including SMP related). You can check improvements in Release Notes
document (sect.What's New?, New Features) included in linux documntation package given on below link
For example latest uboot has defines for most severe arm errara like #define CONFIG_ARM_ERRATA_743622 and so on
uboot/include/configs/mx6_common.h
mx6_common.h\configs\include - uboot-imx - i.MX U-Boot
Best regards
igor