gpio_key and QT5.6 KO

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

gpio_key and QT5.6 KO

1,642件の閲覧回数
xavierrazavet
Contributor I

Hello,

I have a problem with gpio_key and Qt5.6, no problem with Qt4.8.

My configuration is buildroot2016.05 with kernel 3.10.17 and Qt5.6 for now + imx6dl

In device tree, the gpio is set to recover the key you want in Qt application. For exemple, Key_Up (103d or 0x67) as below:

   gpio_keys {
        compatible = "gpio-keys";
        #address-cells = <1>;
        #size-cells = <0>;

        Key_Up {
                label = "Key_Up";
                linux,code = <103>;
                gpios = <&gpio4 12 4>;  /* 4 = active high level-sensitive */
        };

...

In Qt4.8 configuration, there is the package BR2_PACKAGE_QT_KEYBOARD_TTY=y which is included.

But this package does not exist anymore under Qt5.6. I suppose it is ok under Qt4.8 due to this package.

remark: with the command "hexdump -C /dev/input/event1", i can see the IO ON/OFF on the KEY_Up (103d or 0x67) as below:

00000000  3f 2b 00 00 6f e2 09 00  01 00 67 00 00 00 00 00  |?+..o.....g.....|
00000010  3f 2b 00 00 6f e2 09 00  00 00 00 00 00 00 00 00  |?+..o...........|

00000020  40 2b 00 00 f5 56 01 00  01 00 67 00 01 00 00 00  |@+...V....g.....|
00000030  40 2b 00 00 f5 56 01 00  00 00 00 00 00 00 00 00  |@+...V..........|

This command shows the kernel is OK.

Someone has an idea.

Thanks in advance for your help.

Best Regards.

0 件の賞賛
返信
3 返答(返信)

1,506件の閲覧回数
xavierrazavet
Contributor I

Hello All,

 A first solution is to add as argument, « -plugin evdevkeyboard:/dev/input/event1 » :

./Application -platform linuxfb -plugin evdevkeyboard:/dev/input/event1

May be another exists ?

Regards

0 件の賞賛
返信

1,506件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hello Xavier,

thank you for sharing your solution, I will check with applications enginers for an alternative solution.

Regards,

Carlos

0 件の賞賛
返信

1,506件の閲覧回数
xavierrazavet
Contributor I

Hello Carlos,

Thank you for your reply.

A remark concerning eventX.

eventX = event0 as application argument if you have not physical keyboard

eventX = event1 as application argument if you have already a physical keyboard plugged

Best Regards,

Xavier

0 件の賞賛
返信