gicv3 interrupt init, interrupt trigger, interrupt handler at bl31 ATF ( EL3 mode )

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

gicv3 interrupt init, interrupt trigger, interrupt handler at bl31 ATF ( EL3 mode )

1,390件の閲覧回数
dongjoo99kim
Contributor I

Dear all.

 

I have developed imx8mq including cortex a53, gicv3 controller.

 

As i know, bl31 in ATF can boot at EL3 mode, and bl31 in ATF can use fiq using gicv3.

If my understand is not correct, Please. correct me.

 

As i know, bl31 in ATF just use fiq triggered by other sw as like kernel ( non secure EL1 ) or Trust OS ( secure EL1 )  

If my understand is not correct, Please. correct me.

 

I want to enable gicv3 interrupt init, interrupt trigger, interrupt handler at bl31 in ATF ( EL3 mode ) 

For example, after trigger interrupt at bl31 in ATF, I want to check the interrupt handler by bl31 exception vector table at bl31 in ATF.

 

I confuse the concept about irq and fiq.

Do the bl31 int ATF use only  firq not irq ? 

 

If bl31 in ATF use only firq, Could you share to me the method how to enable the fiq in bl31? 

And, Could you share to me the method how to check the interrupt handler by bl31 exception vector table ?

 

If bl31 interrupt handler is triggered by bl31 exception vector table,

Could you share to me the location about bl31 exception vector table ?

 

Thanks.

0 件の賞賛
返信
1 返信

1,380件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

 

Suggest you research the interrupt design in ATF: docs/design/interrupt-framework-design.rst

bl31/aarch64/runtime_exceptions.S

bl31/aarch64/bl31_entrypoint.S

	el3_entrypoint_common					\
		_init_sctlr=1					\
		_warm_boot_mailbox=!PROGRAMMABLE_RESET_ADDRESS	\
		_secondary_cold_boot=!COLD_BOOT_SINGLE_CPU	\
		_init_memory=1					\
		_init_c_runtime=1				\
		_exception_vectors=runtime_exceptions		\
		_pie_fixup_size=BL31_LIMIT - BL31_BASE

 

0 件の賞賛
返信