Hi @m_selukar,
Thank you for your reply.
I have reviewed this case in detail, and it seems that the problem is related to your display resolution.
The i.MX8QM supports two displays with an interface LVDS to HDMI with a resolution up to 1920x1080.
Your ASUS ProArt PA147CDV has a resolution 1920x550 that must be properly managed by the processor. However, the driver that implements the LVDS to HDMI converter and the signals for the HDMI output supports by default the resolutions provided in the standard CEA 861.
Unfortunately, 1920x550 is not part of these resolutions and you will need to customize the drivers to acquire this value.
Is important to say that this customization requires a great effort and also may present issues with the implementation on Android.
Please have a look on the following thread:
Re: Multi-display support on iMX8QM running Androi... - NXP Community
You could find the drivers mentioned on that thread here:
Driver for IT6263 (IC used in the LVDS to HDMI converter)
linux-imx/drivers/gpu/drm/bridge/it6263.c at lf-6.1.y · nxp-imx/linux-imx · GitHub
EDID
linux-imx/drivers/gpu/drm/drm_edid.c at lf-6.1.y · nxp-imx/linux-imx · GitHub
I hope this information will be helpful.
Have a great day!