get cpu revision

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

get cpu revision

1,890件の閲覧回数
mm2021
Contributor III

I'd like to get the cpu revision. I know in linux, cat /proc/cpuinfo & lscpu can list some information of CPU. but seems cannor list the cpu revision.

root@imx8mmab2:~/audio_files# lscpu
Architecture: aarch64
CPU op-mode(s): 32-bit, 64-bit
Byte Order: Little Endian
CPU(s): 4
On-line CPU(s) list: 2,3
Off-line CPU(s) list: 0,1
Thread(s) per core: 1
Core(s) per socket: 2
Socket(s): 1
NUMA node(s): 1
Vendor ID: ARM
Model: 4
Model name: Cortex-A53
Stepping: r0p4
BogoMIPS: 16.00
NUMA node0 CPU(s): 2,3
Vulnerability Itlb multihit: Not affected
Vulnerability L1tf: Not affected
Vulnerability Mds: Not affected
Vulnerability Meltdown: Not affected
Vulnerability Spec store bypass: Not affected
Vulnerability Spectre v1: Mitigation; __user pointer sanitization
Vulnerability Spectre v2: Not affected
Vulnerability Srbds: Not affected
Vulnerability Tsx async abort: Not affected
Flags: fp asimd evtstrm aes pmull sha1 sha2 crc32 cpuid
root@imx8mmab2:~/audio_files# cat /proc/cpuinfo
processor : 2
BogoMIPS : 16.00
Features : fp asimd evtstrm aes pmull sha1 sha2 crc32 cpuid
CPU implementer : 0x41
CPU architecture: 8
CPU variant : 0x0
CPU part : 0xd03
CPU revision : 4

processor : 3
BogoMIPS : 16.00
Features : fp asimd evtstrm aes pmull sha1 sha2 crc32 cpuid
CPU implementer : 0x41
CPU architecture: 8
CPU variant : 0x0
CPU part : 0xd03
CPU revision : 4

root@imx8mmab2:~/audio_files#

 

0 件の賞賛
返信
0 返答(返信)