gdb setup for imx287 evk

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

gdb setup for imx287 evk

2,127件の閲覧回数
ask
Contributor III

I am trying to setup the gdb setup for imx287 evk board as per the attached document.  gdb version I used is 7.4.

I struck at step no 6 in the section 4, i.e not able to build native version(including gdb server).

Please can any one help out by providing the commands for the step no 6. In the document it has been given for imx6.

0 件の賞賛
返信
1 返信

1,963件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi ashok

I think you can try below steps for i.MX23

Debugging the iMX233-OLinuXino via SJTAG with OpenOCD — Christian's Blog

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信