g2d conversion for RGB24 to RGB565

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

g2d conversion for RGB24 to RGB565

2,953件の閲覧回数
saurabh206
Senior Contributor III

Hi

Does g2d is able to do color space conversion between RGB24 to RGB565?

Also does g2d is used to do re-size RGB24 to RGB24?

Thanks

Saurabh

タグ(2)
0 件の賞賛
返信
2 返答(返信)

2,585件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Saurabh

I am afraid not, as suggests description in attached

Graphics Guide sect.2.4.1 Color space conversion from YUV to RGB

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,585件の閲覧回数
saurabh206
Senior Contributor III

Hi igor,

Thanks for reply.

What is a significance of 2.2.7

pastedImage_0.png

Is there any alternate method to do RGB to RGB scaling other than IPU?

Thanks,

Saurabh

0 件の賞賛
返信