g_ether/RNDIS not stable

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

g_ether/RNDIS not stable

1,658件の閲覧回数
Pav
Contributor I

Hello,

we are using 2.6.28 kernel on i.mx25. I am trying to establish RNDIS connection with Win XP computer.

It works on majority of XP SP3 computers, however not on all of them. On some computers I get 'Cannot start driver' (code 10) error. RNDIS driver is ver. 5.1.2600.5512 everywhere.

There is also a computer with XP SP2. I tried installing hotfix as suggested in 

http://www.droidforums.net/forum/tech-issues-bug-reports-suggestions/66688-solution-windows-xp-sp2-l...

unfortunately without success.

Quite often I see kernel panic:

[4294742.714000] Unable to handle kernel NULL pointer dereference at virtual address 00000002
[4294742.714000] pgd = c0004000
[4294742.714000] [00000002] *pgd=00000000
[4294742.714000] Internal error: Oops: 17 [#1] PREEMPT

Seems that it happens if the board is connected to USB1.1 port after I install driver and unplug the device.

Does anybody know about the state of the RNDIS driver on the Linux side, which windows versions it is supposed to work with? Will updating to 2.6.31 solve the issue?

Thanks.

タグ(2)
0 件の賞賛
返信
0 返答(返信)