.fw.ihex file for IMX6SL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

.fw.ihex file for IMX6SL

9,718 Views
Harris
Contributor II

How to generate a .fw.ihex on the IMX6SL platform.

Thanks.

Labels (1)
18 Replies

9,255 Views
art
NXP Employee
NXP Employee

Refer to the Section 10.3.7 of the attached document for the information on how to convert a .fw file to .fw.ihex one. Also, here you can find the ihex2bin.py script mentioned, if required:

Splash screen on EPD in u-boot

Best Regards,

Artur

0 Kudos
Reply

9,255 Views
Harris
Contributor II

Hi, Artur,

I can not get the ihex2bin.py in your answer.

Thanks.

Harris

0 Kudos
Reply

9,255 Views
art
NXP Employee
NXP Employee

Go to the following thread:

Splash screen on EPD in u-boot

You can download the script from there.

Artur

0 Kudos
Reply

9,255 Views
Harris
Contributor II

FYI.

Thanks.

0 Kudos
Reply

9,255 Views
art
NXP Employee
NXP Employee

Please find attached the resulting .fw file.

Best Regards,

Artur

9,255 Views
Harris
Contributor II

Dear Artur,

I think I need the .fw.ihex not .fw.

Would you please help me transfer a .fw.ihex file for me.

Thanks.

0 Kudos
Reply

9,255 Views
Harris
Contributor II

Many Thanks.

0 Kudos
Reply

9,255 Views
art
NXP Employee
NXP Employee

Are you logged into the community? If so, press the "Add Comment" button, then push the "Use advanced editor" link on the right upper corner of the message window, then, after the advanced editor script is loaded, push "Attach" on the right lower corner of the message window.

If you are not logged into the community, first, create your own account, then log in, and then follow the instructions above.

Artur

0 Kudos
Reply

9,255 Views
Harris
Contributor II

Dear Artur,

Would you please help me to transfer the .fw.ihex?

Thanks.

0 Kudos
Reply

9,255 Views
art
NXP Employee
NXP Employee

I'm in progress :-)

0 Kudos
Reply

9,255 Views
Harris
Contributor II

Hi, Artur,

OK.

Thanks.

0 Kudos
Reply

9,255 Views
Harris
Contributor II

How to insert a file in the reply.

The Web is so difficult for me.

Thanks.

0 Kudos
Reply

9,255 Views
art
NXP Employee
NXP Employee

Unfortunately, I don't understand exactly what kind of data do you mean. Please specify it in more details. Do you mean the waveform file for the i.MX6SL EPD controller?


Have a great day,
Artur

0 Kudos
Reply

9,255 Views
Harris
Contributor II

Hi, Artur,

Yes,  I have the waveform. How to generate the .ihex for IMX6SL EPD.

Thanks.

0 Kudos
Reply

9,255 Views
art
NXP Employee
NXP Employee

Please provide the original .wbf file supplied by the E-ink display vendor and I'll convert it to .fw for you.

Best Regards,

Artur

0 Kudos
Reply

9,255 Views
Harris
Contributor II

Hi, Artur,

Sorry for late.

Is there a tool for transfer?

Thanks.

0 Kudos
Reply

9,255 Views
art
NXP Employee
NXP Employee

You can just attach it here.

Regards,

Artur

9,255 Views
Yuri
NXP Employee
NXP Employee

Hello,

  please let us know more details - what kind of file / data do You mean ?

Regards,

Yuri.

0 Kudos
Reply