function confilict

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

function confilict

Jump to solution
2,773 Views
wanglee
Contributor III

Q:How to end this confilict?

1.jpg

2.jpg

3.jpg

Labels (1)
0 Kudos
Reply
1 Solution
2,596 Views
wanglee
Contributor III

  I replaced 4.7kΩ with 18kΩ, the wave form changed. I think the problem is drive strength of EIM signals.so I reconfigured the DSE(drive strength field),but it didn't work. Can you give me some advice?

IMG_20160219_160133.jpgIMG_20160219_163115.jpg

View solution in original post

0 Kudos
Reply
4 Replies
2,596 Views
Yuri
NXP Employee
NXP Employee

Hello,

   The Boot  Configuration Select with resistors just provides 4.7 kΩ pullup, when

the switch is ON. Basically this should not affect EIM signals, if outputs are strong

enough to overdrive 4.7 kΩ.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,596 Views
wanglee
Contributor III

how to make it strong enough?

0 Kudos
Reply
2,596 Views
Yuri
NXP Employee
NXP Employee

Hello,

The following app note helps to setup pin’s electrical properties. 

“Influence of Pin Setting on System Function and Performance”

< http://www.nxp.com/files/32bit/doc/app_note/AN5078.pdf >

Regards,

Yuri.

0 Kudos
Reply
2,597 Views
wanglee
Contributor III

  I replaced 4.7kΩ with 18kΩ, the wave form changed. I think the problem is drive strength of EIM signals.so I reconfigured the DSE(drive strength field),but it didn't work. Can you give me some advice?

IMG_20160219_160133.jpgIMG_20160219_163115.jpg

0 Kudos
Reply