function confilict

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

function confilict

跳至解决方案
2,934 次查看
wanglee
Contributor III

Q:How to end this confilict?

1.jpg

2.jpg

3.jpg

标签 (1)
0 项奖励
回复
1 解答
2,757 次查看
wanglee
Contributor III

  I replaced 4.7kΩ with 18kΩ, the wave form changed. I think the problem is drive strength of EIM signals.so I reconfigured the DSE(drive strength field),but it didn't work. Can you give me some advice?

IMG_20160219_160133.jpgIMG_20160219_163115.jpg

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,757 次查看
Yuri
NXP Employee
NXP Employee

Hello,

   The Boot  Configuration Select with resistors just provides 4.7 kΩ pullup, when

the switch is ON. Basically this should not affect EIM signals, if outputs are strong

enough to overdrive 4.7 kΩ.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
2,757 次查看
wanglee
Contributor III

how to make it strong enough?

0 项奖励
回复
2,757 次查看
Yuri
NXP Employee
NXP Employee

Hello,

The following app note helps to setup pin’s electrical properties. 

“Influence of Pin Setting on System Function and Performance”

< http://www.nxp.com/files/32bit/doc/app_note/AN5078.pdf >

Regards,

Yuri.

0 项奖励
回复
2,758 次查看
wanglee
Contributor III

  I replaced 4.7kΩ with 18kΩ, the wave form changed. I think the problem is drive strength of EIM signals.so I reconfigured the DSE(drive strength field),but it didn't work. Can you give me some advice?

IMG_20160219_160133.jpgIMG_20160219_163115.jpg

0 项奖励
回复