function confilict

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,856件の閲覧回数
wanglee
Contributor III

Q:How to end this confilict?

1.jpg

2.jpg

3.jpg

ラベル(1)
0 件の賞賛
返信
1 解決策
2,679件の閲覧回数
wanglee
Contributor III

  I replaced 4.7kΩ with 18kΩ, the wave form changed. I think the problem is drive strength of EIM signals.so I reconfigured the DSE(drive strength field),but it didn't work. Can you give me some advice?

IMG_20160219_160133.jpgIMG_20160219_163115.jpg

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,679件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

   The Boot  Configuration Select with resistors just provides 4.7 kΩ pullup, when

the switch is ON. Basically this should not affect EIM signals, if outputs are strong

enough to overdrive 4.7 kΩ.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,679件の閲覧回数
wanglee
Contributor III

how to make it strong enough?

0 件の賞賛
返信
2,679件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

The following app note helps to setup pin’s electrical properties. 

“Influence of Pin Setting on System Function and Performance”

< http://www.nxp.com/files/32bit/doc/app_note/AN5078.pdf >

Regards,

Yuri.

0 件の賞賛
返信
2,680件の閲覧回数
wanglee
Contributor III

  I replaced 4.7kΩ with 18kΩ, the wave form changed. I think the problem is drive strength of EIM signals.so I reconfigured the DSE(drive strength field),but it didn't work. Can you give me some advice?

IMG_20160219_160133.jpgIMG_20160219_163115.jpg

0 件の賞賛
返信