fsl-mm-codecs source availability

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

fsl-mm-codecs source availability

ソリューションへジャンプ
2,744件の閲覧回数
bonzo
NXP Employee
NXP Employee

Is the source code for the fsl-mm-codecs available for the iMX53?

I have a customer that would to recompile the libraries with with the hard float option.

Is this source code Freescale's, or was it provided by the IP vendor?

ラベル(2)
0 件の賞賛
返信
1 解決策
2,454件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

No, the source code is not available, if your customer wants to recompile, he would need to check with each IP vendor of each codec.

Hope this helps!

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,454件の閲覧回数
bonzo
NXP Employee
NXP Employee

Is there anyway we could have this library recompiled with hard float?

0 件の賞賛
返信
2,455件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

No, the source code is not available, if your customer wants to recompile, he would need to check with each IP vendor of each codec.

Hope this helps!

0 件の賞賛
返信