fsl-mm-codecs source availability

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

fsl-mm-codecs source availability

Jump to solution
2,706 Views
bonzo
NXP Employee
NXP Employee

Is the source code for the fsl-mm-codecs available for the iMX53?

I have a customer that would to recompile the libraries with with the hard float option.

Is this source code Freescale's, or was it provided by the IP vendor?

Labels (2)
0 Kudos
Reply
1 Solution
2,416 Views
SergioSolis
NXP Employee
NXP Employee

No, the source code is not available, if your customer wants to recompile, he would need to check with each IP vendor of each codec.

Hope this helps!

View solution in original post

0 Kudos
Reply
2 Replies
2,416 Views
bonzo
NXP Employee
NXP Employee

Is there anyway we could have this library recompiled with hard float?

0 Kudos
Reply
2,417 Views
SergioSolis
NXP Employee
NXP Employee

No, the source code is not available, if your customer wants to recompile, he would need to check with each IP vendor of each codec.

Hope this helps!

0 Kudos
Reply