fsl-flexspi is missing in imx8qmmek Yocto Zeus branch?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

fsl-flexspi is missing in imx8qmmek Yocto Zeus branch?

1,775件の閲覧回数
stuartrubin
Contributor III

We are developing code for the imx8qmmek which requires access to the SPI drivers. Previously, we had been using the old Warrior branch of Yocto BSP Linux. The applicable driver was fsl-flexspi (located in /build-xwayland/tmp/work-shared/imx8qxpmek/kernel-source/drivers/mtd/spi-nor/fsl-flexspi.c).

For a variety of reasons, we have moved to the Zeus branch of code. The driver (fsl-flexspi.c) is missing. 

Can someone please explain if it was removed, or renamed, or if I need to somehow enable it in the source? I did not see the option to use this driver in the "menuconfig" when configuring Linux.

Thank you!

0 件の賞賛
返信
2 返答(返信)

1,766件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi stuartrubin

 

zeus flexspi driver can be found on

https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/spi/spi-nxp-fspi.c?h=imx_5.4.47_2....

 

Best regards
igor

1,755件の閲覧回数
stuartrubin
Contributor III

Thank you, Igor. I could not find it because it was both renamed and moved!

0 件の賞賛
返信