fsl-flexspi is missing in imx8qmmek Yocto Zeus branch?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

fsl-flexspi is missing in imx8qmmek Yocto Zeus branch?

1,764 次查看
stuartrubin
Contributor III

We are developing code for the imx8qmmek which requires access to the SPI drivers. Previously, we had been using the old Warrior branch of Yocto BSP Linux. The applicable driver was fsl-flexspi (located in /build-xwayland/tmp/work-shared/imx8qxpmek/kernel-source/drivers/mtd/spi-nor/fsl-flexspi.c).

For a variety of reasons, we have moved to the Zeus branch of code. The driver (fsl-flexspi.c) is missing. 

Can someone please explain if it was removed, or renamed, or if I need to somehow enable it in the source? I did not see the option to use this driver in the "menuconfig" when configuring Linux.

Thank you!

0 项奖励
回复
2 回复数

1,755 次查看
igorpadykov
NXP Employee
NXP Employee

Hi stuartrubin

 

zeus flexspi driver can be found on

https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/spi/spi-nxp-fspi.c?h=imx_5.4.47_2....

 

Best regards
igor

1,744 次查看
stuartrubin
Contributor III

Thank you, Igor. I could not find it because it was both renamed and moved!

0 项奖励
回复