ffmpeg command for live video with mipi csi2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ffmpeg command for live video with mipi csi2

2,039件の閲覧回数
srinivasaporam
Contributor II

Hi,

We have got imx6Q board with which ov5647 (raspi camera) is interfaced through mipi csi2 and we are using linux-linaro stable kernel source.

When we are using following command:

ffmpeg -pix_fmt bayer_bggr8 -f v4l2 -s 1280x960 -i /dev/video0 -c:v libx264 -preset ultrafast ~/Desktop/1234.avi

then 1234.avi video file is being created on Desktop which we can able to play. Now if we want to take live video from the raspi camera and to display that on desktop , what is command in ffmpeg (like raspivid -t 10000, which displays live video on raspberry pi board)

ラベル(5)
0 件の賞賛
返信
1 返信

1,717件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Srinivasa

seems this is special ffmpeg question, suggest to post this on ffmpeg

mailing list

https://www.ffmpeg.org/contact.html#MailingLists

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信