feed RTC_XTALI with square wave

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

feed RTC_XTALI with square wave

Jump to solution
2,561 Views
chris321
Contributor IV

Hello Community,

I did not found anything about this in the datasheet.

Is it possible to feed the (analog) pin RTC_XTALI from the i.MX28 with a square wave?

For example the square wave output from an external RTC.

Best Regards

Labels (1)
0 Kudos
Reply
1 Solution
2,418 Views
4guin4g4
Contributor IV

Yes, a squared wave can feed the RTC_XTALI. yous be sure that it meets the specs in the RM:

"Since the internal RTC circuitry is powered from VDDXTAL which

voltage level is around 1.0V, the input 32K clock signal level on  RTC_XTALI should be 1V also. "

View solution in original post

0 Kudos
Reply
3 Replies
2,419 Views
4guin4g4
Contributor IV

Yes, a squared wave can feed the RTC_XTALI. yous be sure that it meets the specs in the RM:

"Since the internal RTC circuitry is powered from VDDXTAL which

voltage level is around 1.0V, the input 32K clock signal level on  RTC_XTALI should be 1V also. "

0 Kudos
Reply
2,418 Views
chris321
Contributor IV

Thank you Carlos,

I do not want to embarrass myself, but in wich Reference Manual did you found this sentence?

The downloadable version is Rev. 1, 2010, in this version I did not found it.

If I feed the XTALI with a 1V squared wave, what about the XTALO? Put it to GND, or let it floated?

0 Kudos
Reply
995 Views
WSLJ
Contributor I
0 Kudos
Reply