failed to execute child process xterm (no such file or directory)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

failed to execute child process xterm (no such file or directory)

4,476 Views
sachusanal
Contributor III

Hai Sir ,

I have crosscompiled Qt application for IMX6qsabresd board.

while running executable in board i get an error like  failed to execute child process xterm (no such file or directory)

i am using core-imag-sato-sdk image in board. if it is the problem of the image

could you please help me solve this issue.

Regards

Sachu

Labels (1)
0 Kudos
Reply
1 Reply

2,641 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Sachu,

I’m afraid that Freescale does not support QT code. However, you could refer to the following document from the Community:

Setting up Qt Creator to build for i.MX6

Hope this will be useful for you.

Please accept our apologies for any inconveniences this may cause.

Best regards!

/Carlos

0 Kudos
Reply