ext4 encryption

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ext4 encryption

6,453 Views
bba
Contributor III

Hello, please find attached some remarks on ext4 encryption on i.MX6UL EVK using Yocto build fslc community kernel version 4.3.0

 

Ext4 encryption is supported by mainline kernel version 4.1.3 or higher. Encryption keys are stored in the keyring. To get started, make sure you have enabled

CONFIG_KEYS and CONFIG_EXT4_ENCRYPTION kernel options. Furthermore you need to update e2fsprogs to at least version 1.43. I prefer the sources from git repository.

 

https://wiki.archlinux.org/index.php/Ext4#Using_ext4_per_directory_encryption

 

Ok, I'm using the latest fslc kernel from meta-fsl-arm at version 4.3.0

 

root@imx6ulevk:~# uname -a

Linux imx6ulevk 4.3.0-fslc+g5a86d64 #1 SMP Wed Jan 6 10:21:10 CET 2016 armv7l GNU/Linux

 

Updating the e2fsprogs recipe you can use the attached file. Here you have to replace the contents of yocto/poky/meta/recipes-devtools/e2fsprogs

 

Now build your image, copy it to an mircoSdCard and run the system on the i.MX6UL evaluationboard. Login via serial debug or ssh if possible.

 

First generate a random salt (or use an simple salt). Than create the key in the keyring and use it to set the policy for the directory to be encrypted.

 

root@imx6ulevk:~# e4crypt add_key -S 0x1234

Enter passphrase (echo disabled):

Added key with descriptor [7c36eecef6c5ee9e]

 

root@imx6ulevk:~# e4crypt set_policy 7c36eecef6c5ee9e /encrypted/dir

Key with descriptor [7c36eecef6c5ee9e] applied to /encrypted/dir.

 

root@imx6ulevk:~# touch /encrypted/dir/test.txt

 

root@imx6ulevk:~# ls -l /encrypted/dir/

-rw-r--r-- 1 root root 0 Jan 4 10:52 test.txt

 

After each reboot, the same command can be used set the key for decryption of the directory and its descendants.

 

root@imx6ulevk:~# ls -l /encrypted/dir/

-rw-r--r-- 1 root root 0 Jan 4 10:52 z,x7tfUEMLzh+AU2MkQcnB

 

root@imx6ulevk:~# e4crypt get_policy /encrypted/dir/

/encrypted/dir/: 7c36eecef6c5ee9e

 

root@imx6ulevk:~# e4crypt add_key -S 0x1234

Enter passphrase (echo disabled):

Added key with descriptor [7c36eecef6c5ee9e]

 

root@imx6ulevk:~# ls -l /encrypted/dir/

-rw-r--r-- 1 root root 0 Jan 4 10:52 test.txt

 

That's all.

Original Attachment has been moved to: e2fsprogs.tar.gz

Labels (2)
Tags (1)
0 Kudos
Reply
2 Replies

4,520 Views
DavisRoman
Contributor III

Hello,

I would also like to enable ext4 encryption on our product.

Our kernel has CONFIG_KEYS and CONFIG_EXT4_ENCRYPTION enabled. Also, I made sure to have an updat to date version of e2fsprogs. We're using version 1.43.8.

Unfortunately, I get a kernel panic whenever I try the above steps show below.

Any ideas what the issue could be?

Thank you!

-Davis

root@target:~# uname -r
4.1.15+ga1644c9
root@target:~# e4crypt add_key -S 0x1234
Enter passphrase (echo disabled):
Added key with descriptor [080b217fb3239f3d]
root@target:~# mkdir testfolder
root@target:~# e4crypt set_policy 080b217fb3239f3d testfolder/
Key with descriptor [080b217fb3239f3d] applied to testfolder/.
root@hon-grip-aio-200-01939A:~# touch testfolder/test.txt
Unable to handle kernel NULL pointer dereference at virtual address 00000000
pgd = 89f8c000
[00000000] *pgd=19f99831, *pte=00000000, *ppte=00000000
Internal error: Oops: 817 [#1] PREEMPT SMP ARM
Modules linked in: art(O) gc2145_camera asix usbnet m25p80 ath9k ath9k_common ath9k_hw ath galcore(O) g_ether usb_f_rndis u_ether libcomposite configfs
CPU: 0 PID: 2414 Comm: touch Tainted: G O 4.1.15+ga1644c9 #1
Hardware name: Freescale i.MX6 Quad/DualLite (Device Tree)
task: 89f86ac0 ti: 8978e000 task.ti: 8978e000
PC is at v7_dma_clean_range+0x20/0x38
LR is at __dma_page_cpu_to_dev+0x28/0x94
pc : [<8001f9e8>] lr : [<8001b8b0>] psr: 000f0013
sp : 8978fbb0 ip : 8bb57000 fp : 8001b960
r10: 885f5810 r9 : 00000000 r8 : 899c7c00
r7 : 00000001 r6 : 00000010 r5 : 8cb57000 r4 : 00000000
r3 : 0000001f r2 : 00000020 r1 : 00000010 r0 : 00000000
Flags: nzcv IRQs on FIQs on Mode SVC_32 ISA ARM Segment user
Control: 10c53c7d Table: 19f8c059 DAC: 00000015
Process touch (pid: 2414, stack limit = 0x8978e210)
Stack: (0x8978fbb0 to 0x89790000)
fba0: 8001fa38 00000010 00000000 8cb57000
fbc0: 885f5810 00000000 00000000 8001b9d0 00000000 00000000 80bbb424 8058f33c
fbe0: 00000001 00000000 ffffffff 00000010 8978fc7c 000000d0 8978fc5c 80c661c4
fc00: 8978fc3f 00000000 8978fc5c 899cbf80 899c7c00 88bbf800 885f5810 8978fc7c
fc20: 8768ad34 89f3808e 8978fc5c 8058f740 00000000 802bf780 600f0013 ffffffff
fc40: 8978fce8 899cbf80 899c7c00 00000000 8978fc6c 801b4f50 8026d444 8bc95702
fc60: 0000008e 00000040 19f3808e 8bc44142 00000d34 00000040 1768ad34 00000000
fc80: 00000000 8978fc84 8978fc84 00000000 89f38000 00000000 8768ab40 89f38000
fca0: 80bc9f98 00000001 87ca1e84 8768ab40 8790d1c0 801b5114 0000001c 807c2304
fcc0: 00000001 7865cc54 303a3474 32623038 62663731 39333233 00643366 00040101
fce0: 7f210b08 3d9f23b3 c1628c21 38e4fa62 220a5aee dd6769bf 8602a400 00000001
fd00: 8768ab40 000000ff 00000008 801b5768 96163000 00001000 00000000 80183f24
fd20: 00000000 00000000 00000000 8768ab40 00000001 8790d1c0 00000002 00000000
fd40: 00000000 00000000 8790d1c0 00000001 00000000 00000001 8768ab40 00000001
fd60: 00000001 00000001 00000000 80184304 87ca1e70 00000000 8978fe04 898ba528
fd80: 80c15c84 89768000 87ca1e70 8978fe04 00000000 809a6398 8790d1c0 898ba528
fda0: 0000004b 89740000 8790d1c0 00000000 00000020 00000001 0002cbec 80bb55a0
fdc0: 88001500 80bb66f4 0002cbec 87ca1e58 87ca1e58 87ca1aa0 8768ab40 8978feb0
fde0: 8768ab40 87ca1aa0 87ca1e58 80184628 87ca1af0 87ca1e58 0002cbec 807c21ac
fe00: 87ca1aa0 00000000 00000000 87ca1e58 8978ff74 87ca1aa0 00020941 800f5170
fe20: 8978fef0 8978ff74 87ca1aa0 800f9a7c 88b13000 800f7abc 00000000 00000022
fe40: 898ee3c0 00000000 00000000 00000001 88aad610 87ca1aa0 8768ab40 899cb180
fe60: 01bc60c0 8978ff74 88b13000 898ee3c0 8978fef0 00000000 8978ff74 88b13000
fe80: 8978feb0 00000000 0002cbec 800f9fa0 8978feac 88b13000 00000000 8978ffb0
fea0: 89740000 80000007 76f482ec 00000000 898badc0 89740038 00000054 8001ce58
fec0: 00000000 8978ff74 00000001 ffffff9c 88b13000 8000f604 8978e000 00000000
fee0: 0002cbec 800fb320 00000041 80bbb714 88aad610 87ca1aa0 f0bf2f52 00000008
ff00: 88b1301b 0002cc14 00000000 80009338 8768ab40 00000301 00000004 00000258
ff20: 00000000 00000000 00000000 807c21ac 00000003 80107368 80bb6760 00020941
ff40: 00000000 00020941 ffffff9c 88b13000 00000005 00000003 ffffff9c 88b13000
ff60: 00000005 800ec778 89f86eb8 0046c000 89740000 00020941 897481b6 00000022
ff80: 00000300 00000001 76fc0000 00000941 00000000 7eac4de4 00000005 8000f604
ffa0: 8978e000 8000f480 00000941 00000000 7eac4eee 00020941 000001b6 00000000
ffc0: 00000941 00000000 7eac4de4 00000005 7eac4eee 00000001 0002cc14 0002cbec
ffe0: 76f482ec 7eac4b80 000128bc 76f48340 600e0010 7eac4eee 00000000 00000000
[<8001f9e8>] (v7_dma_clean_range) from [<8001b8b0>] (__dma_page_cpu_to_dev+0x28/0x94)
[<8001b8b0>] (__dma_page_cpu_to_dev) from [<8001b9d0>] (arm_dma_map_page+0x70/0x74)
[<8001b9d0>] (arm_dma_map_page) from [<8058f33c>] (ablkcipher_edesc_alloc.constprop.1+0x180/0x568)
[<8058f33c>] (ablkcipher_edesc_alloc.constprop.1) from [<8058f740>] (ablkcipher_encrypt+0x1c/0x90)
[<8058f740>] (ablkcipher_encrypt) from [<801b4f50>] (ext4_derive_key_aes+0x104/0x15c)
[<801b4f50>] (ext4_derive_key_aes) from [<801b5114>] (ext4_generate_encryption_key+0x16c/0x1bc)
[<801b5114>] (ext4_generate_encryption_key) from [<801b5768>] (ext4_get_fname_crypto_ctx+0x11c/0x2d4)
[<801b5768>] (ext4_get_fname_crypto_ctx) from [<80183f24>] (search_dir+0x44/0x16c)
[<80183f24>] (search_dir) from [<80184304>] (ext4_find_entry+0x2b8/0x5a8)
[<80184304>] (ext4_find_entry) from [<80184628>] (ext4_lookup+0x34/0x1d8)
[<80184628>] (ext4_lookup) from [<800f5170>] (lookup_real+0x20/0x4c)
[<800f5170>] (lookup_real) from [<800f9a7c>] (do_last+0x7c8/0xc6c)
[<800f9a7c>] (do_last) from [<800f9fa0>] (path_openat+0x80/0x5d8)
[<800f9fa0>] (path_openat) from [<800fb320>] (do_filp_open+0x2c/0x88)
[<800fb320>] (do_filp_open) from [<800ec778>] (do_sys_open+0x108/0x1cc)
[<800ec778>] (do_sys_open) from [<8000f480>] (ret_fast_syscall+0x0/0x3c)
Code: e1a02312 e2423001 e1c00003 e320f000 (ee070f3a)
---[ end trace 87467e4f88b65a79 ]---
Kernel panic - not syncing: Fatal exception
Rebooting in 1 seconds..

U-Boot 2016.03-develop+g500abb6 (Feb 09 2018 - 16:39:09 -0500)

CPU: Freescale i.MX6SOLO rev1.3 at 792 MHz
Reset cause: POR
Board: 
DRAM: 512 MiB
NAND: 0 MiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1
Using default environment

In: serial
Out: serial
Err: serial
facmod value is 1!
Boot Device: EMMC
Net: Board Net Initialization Failed
No ethernet found.
Normal Boot
Hit any key to stop autoboot: 0
=>

0 Kudos
Reply

4,520 Views
fabio_estevam
NXP Employee
NXP Employee

Nice tutorial, thanks!

0 Kudos
Reply