ethernet: Varying network bandwith @TCP/IP stack level

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ethernet: Varying network bandwith @TCP/IP stack level

917 次查看
shajinas
Contributor I

Hello all,

I am working on a custom platform based on i.MX6Q Sabresd SD. The software running on the platform is Yocto BSP kernel version 3.14.28 from Freescale.

The custom platform has an on board ethernet controller which is connected to i.MX6Q via local bus(EIM) and we were  able to establish network connectivity.

I would like to understand on how to vary the network bandwidth at TCP/IP stack level inside kernel. Say for example, I would like to  vary the link bandwidth from Gigabit to 10Mbpps Half/Full Duplex. Many people used ethtool to vary the bandwidth, However it hides the kernel internals.

Any pointers on how to vary the bandwidth @ TCP/IP level would be appreciated.

Thanks

Shajin

标签 (5)
0 项奖励
回复
1 回复

868 次查看
b36401
NXP Employee
NXP Employee

There is nothing special to i.MX.

You can limit network bandwidth using Linux "tc" utility.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复