error when porting android on imx6 sabrelite reg.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

error when porting android on imx6 sabrelite reg.

Jump to solution
5,070 Views
pratikpawar
Contributor II

HI,

          I am trying to port android on imx6 sabrelite by following Android_user_Guide.pdf  i followed the steps mentioned in the document and facing with errors

$ cd ~/myandroid

$ source build/envsetup.sh

$ lunch sabresd_6dq-user

$ make

errors :

  OBJCOPY arch/arm/boot/zImage

  Kernel: arch/arm/boot/zImage is ready

  UIMAGE  arch/arm/boot/uImage

Image Name:   Linux-3.0.35-06114-g3b96084

Created:      Sat Dec 14 11:42:14 2013

Image Type:   ARM Linux Kernel Image (uncompressed)

Data Size:    4709256 Bytes = 4598.88 kB = 4.49 MB

Load Address: 10008000

Entry Point:  10008000

  Image arch/arm/boot/uImage is ready

make[1]: Leaving directory `/home/sasidhar/competency_imx/android/myandroid/kernel_imx'

install -D kernel_imx/arch/arm/boot/uImage  out/target/product/sabresd_6dq/uImage

install -D kernel_imx/arch/arm/boot/zImage  out/target/product/sabresd_6dq/kernel

host Executable: mkfs.ubifs (out/host/linux-x86/obj/EXECUTABLES/mkfs.ubifs_intermediates/mkfs.ubifs)

/usr/bin/ld: skipping incompatible /usr/lib/x86_64-linux-gnu/libz.so when searching for -lz

/usr/bin/ld: skipping incompatible /usr/lib/x86_64-linux-gnu/libz.a when searching for -lz

/usr/bin/ld: skipping incompatible /usr/lib/x86_64-linux-gnu/liblzo2.so when searching for -llzo2

/usr/bin/ld: skipping incompatible /usr/lib/x86_64-linux-gnu/liblzo2.a when searching for -llzo2

/usr/bin/ld: cannot find -llzo2

/usr/bin/ld: skipping incompatible /usr/lib/x86_64-linux-gnu/libuuid.so when searching for -luuid

/usr/bin/ld: skipping incompatible /usr/lib/x86_64-linux-gnu/libuuid.a when searching for -luuid

/usr/bin/ld: cannot find -luuid

/usr/bin/ld: skipping incompatible /usr/lib/x86_64-linux-gnu/libm.so when searching for -lm

/usr/bin/ld: skipping incompatible /usr/lib/x86_64-linux-gnu/libm.a when searching for -lm

/usr/bin/ld: skipping incompatible /usr/lib/x86_64-linux-gnu/libc.so when searching for -lc

/usr/bin/ld: skipping incompatible /usr/lib/x86_64-linux-gnu/libc.a when searching for -lc

collect2: error: ld returned 1 exit status

make: *** [out/host/linux-x86/obj/EXECUTABLES/mkfs.ubifs_intermediates/mkfs.ubifs] Error 1

Please help me to fix these errors.

Thanks & Regards,

Pratik

Labels (2)
0 Kudos
Reply
1 Solution
3,970 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Pratik,

You need to install these packages needed for building android as follows:

$sudo apt-get install uuid uuid-dev  

$sudo apt-get install zlib1g-dev liblz-dev

$sudo apt-get install liblzo2-2 liblzo2-dev

You can have a try. Hope this can help you~~

Best Regards

Dan


View solution in original post

0 Kudos
Reply
10 Replies
3,971 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Pratik,

You need to install these packages needed for building android as follows:

$sudo apt-get install uuid uuid-dev  

$sudo apt-get install zlib1g-dev liblz-dev

$sudo apt-get install liblzo2-2 liblzo2-dev

You can have a try. Hope this can help you~~

Best Regards

Dan


0 Kudos
Reply
3,971 Views
pratikpawar
Contributor II

Hi Dan,

                 Thanks for your suggestions, now its working fine.

Thanks & Regards,

RBT

0 Kudos
Reply
3,971 Views
dreamfly999
Contributor I

Hi Pratik,

I meet the same problem with you. Have you solved by run these commends as Dan post ?

I have tried ,but .......

Could you please share your methods? Thanks a lot.

0 Kudos
Reply
3,971 Views
pratikpawar
Contributor II

Hi Dream,

You can follow the thread https://community.freescale.com/thread/303536

To fix the error, you should install 32 bits lzo2 and luuid to your 64 bits ubuntu.

I installed liblzo2-2_2.05-1_i386.deb ,liblzo2-dev_2.05-1_i386.deb and uuid-dev_2.20.1-1ubuntu3_i386.deb

To install liblzo2

    $ sudo mkdir /usr/lib/liblzo2_i386

    $ sudo dpkg -x liblzo2-dev_2.05-1_i386.deb /usr/lib/liblzo2_i386/

    $ sudo dpkg -x liblzo2-2_2.05-1_i386.deb /usr/lib/liblzo2_i386/

    $ cd /usr/lib/

    $ sudo rm liblzo2.a

    $ sudo rm liblzo2.so

    $ sudo rm liblzo2.so.2

    $ sudo ln -s liblzo2_i386/usr/lib/liblzo2.a liblzo2.a

    $ sudo ln -s liblzo2_i386/usr/lib/liblzo2.so.2.0.0 liblzo2.so

    $ sudo ln -s liblzo2_i386/usr/lib/liblzo2.so.2.0.0 liblzo2.so.2

To install uuid-dev

$ sudo mkdir /usr/lib/uuid-dev

$ sudo dpkg -x uuid-dev_2.20.1-1ubuntu3_i386.deb  /usr/lib/uuid-dev/

$ cd /usr/lib/

$ sudo ln -s uuid-dev/usr/lib/i386-linux-gnu/libuuid.a  libuuid.a

$ sudo ln -s uuid-dev/usr/lib/i386-linux-gnu/libuuid.so  libuuid.so

modify the  external/mtd-utils/mkfs.ubifs/Android.mk.This fixed the "-llzo2 not found; uuid/uuid.h not found;".

$ vi external/mtd-utils/mkfs.ubifs/Android.mk

Remove this flag

LOCAL_LDFLAGS +=-L /usr/lib/x86_64-linux-gnu/

Add the following Flags

LOCAL_LDFLAGS +=-L /usr/lib/

LOCAL_C_INCLUDES +=/usr/lib/uuid-dev/usr/include/

LOCAL_C_INCLUDES +=/usr/lib/liblzo2_i386/usr/include

Thanks & Regards,

Pratik.

0 Kudos
Reply
3,971 Views
dreamfly999
Contributor I

Hi Pratik,

I have build success according to your method. Thanks for sharing :smileyhappy:.

Best Regards

0 Kudos
Reply
3,971 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Dream,

You can also  install 32 bits lzo2 and luuid to your 64 bits ubuntu by commends as follows:

sudo apt-get install liblzo2-dev:i386

sudo apt-get install uuid-dev:i386

Best regards

Dan

0 Kudos
Reply
3,971 Views
dreamfly999
Contributor I

Hi Pratik,

Thanks a lot~~

I will try~~

Best Regards & Merry Christmas

0 Kudos
Reply
3,971 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Pratik,

It's my plessure~~

Since you have solved the problem, I close this DI. If any questions contact  us~~

Best Regards

Dan

0 Kudos
Reply
3,971 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Pratik,

What version of Ubuntu and Android are you using?

Best Regards

Dan

0 Kudos
Reply
3,971 Views
Raybiztech
Contributor V

Can you mention which Version on Android source you are using and what is your source..

0 Kudos
Reply