error running kernel 6.1.1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

error running kernel 6.1.1

1,976 次查看
diegoperez
Contributor II

Hi,

I am getting this error after boot, when I am touching the demos apps, using the last yocto release 6.1.1

 

imx8mp-lpddr4-evk login: [ 18.149542] platform cbtl04gp: deferred probe pending
[ 39.032456] kauditd_printk_skb: 12 callbacks suppressed
[ 39.032465] audit: type=1334 audit(1684939286.584:16): prog-id=0 op=UNLOAD
[ 39.045227] audit: type=1334 audit(1684939286.584:17): prog-id=0 op=UNLOAD
[ 139.769719] GPU[16](ChipModel=0x520 ChipRevision=0x5341):
[ 139.775541] **************************
[ 139.779303] *** GPU STATE DUMP ***
[ 139.783068] **************************
[ 139.786834] axi = 0x0000006E
[ 139.790330] idle = 0x7FFFFFFE
[ 139.793926] FE not idle
[ 139.796739] AQ_HI_CLOCK_CONTROL = 0x00040100
[ 139.801276] DMA appears to be stuck at this address:
[ 139.806417] 0x01007CB8
[ 139.809141] dmaLow = 0xFFFFFF00
[ 139.812655] dmaHigh = 0xFFFFFF00
[ 139.816150] dmaState = 0x00000000
[ 139.819636] command state = 0 (PAR_IDLE_ST)
[ 139.824692] command DMA state = 0 (CMD_IDLE_ST)
[ 139.829748] command fetch state = 0 (FET_IDLE_ST)
[ 139.834808] DMA request state = 0 (REQ_IDLE_ST)
[ 139.839917] cal state = 0 (CAL_IDLE_ST)
[ 139.844984] VE request state = 0 (VER_IDLE_ST)
[ 139.850044] Debug registers:
[ 139.853107] RA[0] debug registers:
[ 139.856867] [00] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 139.865315] [08] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 139.873764] [10] 00000000 00000000 00000000 00000000 00000000

 

Thanks and BR

0 项奖励
回复
2 回复数

1,946 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Is probably that you are playing with the wrong image, download the image again and see if it works.

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

Regards

 

0 项奖励
回复

1,934 次查看
diegoperez
Contributor II

Hi @Bio_TICFSL, the image has been generated by nxp yocto 6.1.1, the board is a design based on evk.

0 项奖励
回复