epdc convert a picture to *.c file

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

epdc convert a picture to *.c file

2,201 次查看
yan2anfei
Contributor III

hi nxp fae,

    I have a imx7dsabre board and a IMXEBOOKDC4 .

somefile like "fsl_rgb_480x360.c" is include In the "mxc_epdc_v2_fb_test.c" file.as follow

#include "ginger_rgb_800x600.c"
#include "fsl_rgb_480x360.c"
#include "colorbar_rgb_800x600.c"

Is there any  tool can convert a picture to *.c file.

标签 (2)
0 项奖励
回复
2 回复数

1,999 次查看
karolmlynczak
Contributor II

Hi yan2.

You can use uC/GUI-BitmapConvert.

0 项奖励
回复

1,999 次查看
igorpadykov
NXP Employee
NXP Employee

Hi yan2

I am afraid such tool is not available.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复