epdc convert a picture to *.c file

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

epdc convert a picture to *.c file

2,207 Views
yan2anfei
Contributor III

hi nxp fae,

    I have a imx7dsabre board and a IMXEBOOKDC4 .

somefile like "fsl_rgb_480x360.c" is include In the "mxc_epdc_v2_fb_test.c" file.as follow

#include "ginger_rgb_800x600.c"
#include "fsl_rgb_480x360.c"
#include "colorbar_rgb_800x600.c"

Is there any  tool can convert a picture to *.c file.

Labels (2)
0 Kudos
Reply
2 Replies

2,005 Views
karolmlynczak
Contributor II

Hi yan2.

You can use uC/GUI-BitmapConvert.

0 Kudos
Reply

2,005 Views
igorpadykov
NXP Employee
NXP Employee

Hi yan2

I am afraid such tool is not available.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply