Hello, I have an application that is responsible for viewing video with gstreamer.
The main application is shown in /dev/fb0 and the video in fb1.
I have configured fb0 to be the foreground and I also configure the color key to show the video that is in the background.
The problem is that I enable the color key only when I'm going to play video and I disable it when there is no video.
When I play the video I have the following Warning:
imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_5 = 0x08000000
imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00100000
imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_5 = 0x00800000
What would be the right way to do this and avoid warnings?
This warning does not appear if I always leave enabled the color_key.
So I think the problem is to enable/disable the color_key in runtime.
Thanks!